CW cannot detect on board USBDM of DEVKIT-S12XE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW cannot detect on board USBDM of DEVKIT-S12XE

跳至解决方案
1,701 次查看
Eric_t
Contributor III

Hi,

CW 5.1 & CW 5.2 cannot detect on board USBDM of DEVKIT-S12XE.

Device manager detects USBDM:

Eric_t_0-1664579938093.png

pemicro firmware updater detects USBDM (I have updated USBDM with the latest firmware):

Eric_t_1-1664580021781.png

CW cannot detect USBDM

Eric_t_2-1664580376572.png

 

When I press the button "Open BDM" it gives the following message:

Eric_t_3-1664580454624.png

 

USBDM status gives the following:

Eric_t_4-1664580530953.png

Since device manager, and pemicro firmware updater is able to upgrade the USBDM with the latest firmware, the on board USBDM works properly. Also I have installed the latest drivers of pemicro.

Does anyone faced the same problem?

Thank you

 

0 项奖励
回复
1 解答
1,672 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Eric_t,

CW5.2 works on Win10

CW5.1 on older Windows

So, what version of Windows do you have?

It looks like you use an old version of the Utility.

I tested with the below firmware on Win10, CW5.2, S12XE100 DevKit.

danielmartynek_0-1664890941689.png

 

BR, Daniel

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,662 次查看
Eric_t
Contributor III

Hi danielmartynek

I was using codewarrior 5.1

I have installed 5.2 and now the on board USBDM works properly

1,673 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Eric_t,

CW5.2 works on Win10

CW5.1 on older Windows

So, what version of Windows do you have?

It looks like you use an old version of the Utility.

I tested with the below firmware on Win10, CW5.2, S12XE100 DevKit.

danielmartynek_0-1664890941689.png

 

BR, Daniel

 

0 项奖励
回复