Hi,
CW 5.1 & CW 5.2 cannot detect on board USBDM of DEVKIT-S12XE.
Device manager detects USBDM:

pemicro firmware updater detects USBDM (I have updated USBDM with the latest firmware):

CW cannot detect USBDM

When I press the button "Open BDM" it gives the following message:

USBDM status gives the following:

Since device manager, and pemicro firmware updater is able to upgrade the USBDM with the latest firmware, the on board USBDM works properly. Also I have installed the latest drivers of pemicro.
Does anyone faced the same problem?
Thank you