CPMUAPITR on s12p

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CPMUAPITR on s12p

1,139 Views
sprince
Contributor I

I'm trying to determine if it is possible to use the internal clock on the s12p.  How accurate is the internal clock on the s12p when trimmed at the factory using  CPMUAPITR?   

 

I guess one would have to know what the tolerance is on a typical oscillator.  If an oscillator has a frequency of 4Mhz and a tolerance of 100ppm, does this mean 4Mhz+/- .01%?  If so, the internal oscillator would have to be trimmed extremely well to be similar.  If it is similar to s08 products, the accuracy is around +/-5%.  Not good enough for my application (need .5%).

 

thanks in advance

 

sp

 

Labels (1)
0 Kudos
Reply
1 Reply

663 Views
Fast
Contributor V

Why not add the external crystal, I think this is cheaper than testing every unit at say 0 and +50degC to calibrate both internal die temperature and internal oscillator, but +/-1.5% is good enough except perhaps for 1Mbit/sec CAN.

 

The cost and toughness advantage of no crystal are attractive especially in hostile environments where this part excels.  Like all engineering you must balance price and performance.

 

Fast55 

 

0 Kudos
Reply