CLI command for codewarrior 10.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLI command for codewarrior 10.7

1,448件の閲覧回数
pratibhasurabhi
Contributor V

Hi ,

I am currently using codewarrior 10.7 on windows 10 - 64bit os. 

I need to automate below process in one go through CLI commands of codewarrior development studio.

1)    open the Codewarrior sw and at the start select the Workspace through CLI and enter in the

        code warrior development studio.

       pratibhasurabhi_0-1611910644187.pngpratibhasurabhi_0-1611910644187.png

2)  Import the project through CLI command.

pratibhasurabhi_0-1611913979027.pngpratibhasurabhi_0-1611913979027.png

3) After project is imported through CLI command need to access "Add Files..."                                         command to add .c file in the project workspace.

           pratibhasurabhi_1-1611914034678.pngpratibhasurabhi_1-1611914034678.png

Please suggest me the respective CLI command for these process to be implemented through CLI.

 

0 件の賞賛
返信
0 返答(返信)