CLI command for codewarrior 10.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLI command for codewarrior 10.7

1,473 Views
pratibhasurabhi
Contributor V

Hi ,

I am currently using codewarrior 10.7 on windows 10 - 64bit os. 

I need to automate below process in one go through CLI commands of codewarrior development studio.

1)    open the Codewarrior sw and at the start select the Workspace through CLI and enter in the

        code warrior development studio.

       pratibhasurabhi_0-1611910644187.png

2)  Import the project through CLI command.

pratibhasurabhi_0-1611913979027.png

3) After project is imported through CLI command need to access "Add Files..."                                         command to add .c file in the project workspace.

           pratibhasurabhi_1-1611914034678.png

Please suggest me the respective CLI command for these process to be implemented through CLI.

 

0 Kudos
Reply
0 Replies