CAN messages missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN messages missing

2,369件の閲覧回数
rahulkrishna
Contributor IV

Hi everyone,

I have seen an implementation of the CAN driver on the Xgate and the processing on the s12x using the following code. The goal of the project is to do processing on some msgs and direct to other channels some other messages.

 

In the Xgate core

void __interrupt XGATE_CAN_RECEIVE(XGCANstruct * channel)

{

  release[msg_index]=1;

// do some processing

  rxmsg[msg_index].msgID = rxid;

  release[msg_index] =0;

msg_index++;

if(msg_index == 10)

  msg_index=0;

-sif();

}


In the s12x core

void __interrupt CAN1_rxnotificationisr(void)

{

XGATE.xgif_50 = BIT9;

}

 

main()

{

while(1)

{

// some logic here

can_rx();

}

}

void can_rx(void)

{

for(index=0; index<=msg_index; index++)

{

  while(release[index] == 1)

  {

  }

  // do the processing some big logic here

}

msg_index=0;

}

 

i had serious doubts about the above implementation and modified as shown below.

 

Xgate core

void __interrupt XGATE_CAN_RECEIVE(XGCANstruct * channel)

{

// do some processing

rxmsg[l_canrxcounter_u8].msgID = rxid;

-sif();

}

 

S12x core

void __interrupt CAN1_rxnotificationisr(void)

{

l_canrxcounter_u8++;

}

and in the main file

int main(void)

{

while(1)

{

  // some big logic here

  can_rx();

}

 

void can_rx(void)

{

  if(l_canrxcounter_u8 > 0)

  {

    //do the message processing

    rxmsg[l_canrxcounter_u8-1];

    l_canrxcounter_u8--;

     // do processing on

    }

}

 

I have written the variable l_canrxcounter_u8 as the shared variable between the two cores without semaphores. Please help me if it is correct and do i need to implement using semaphores. How should i ensure that i am not missing any messages, because in the first implementation i saw that a lot of messages are received but not all by passed to other channels, some messages are missing and also not immediately after the message received it is happening after some messages.

For example

Channel1: msg1 rxed

channel1:msg2 rxed

channel2: msg1 txed

channel1:msg3 rxed

channel1: msg4 rxed

channel2: msg2 txed.

after that the sequence is completely missing. Please help me.   

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,236件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

i would like to provide you some examples I made for CAN at S12XE device. I usually do not use semaphores because of approach to example, however, if it is necessary then PIT example presents how to do it.

best regards,

Ladislav

0 件の賞賛
返信

2,236件の閲覧回数
rahulkrishna
Contributor IV

Thank you very much i will go through the code. If i have any clarifications in the code can you help me out.

0 件の賞賛
返信

2,236件の閲覧回数
kef2
Senior Contributor V

You need to use HW semaphore in your case (where both cores write to the same variable). In multiCPU application++ and -- are not atomic operations. Even though S12X CPU can do ++ or -- using single CPU instruction, this instruction involves 1) reading variable to CPU, 2) calculating new value of variable, and 3) writing new calculated value back to vatiable. XGATE core may read or write the same variable at any stage. Without semaphore it easily may look like some ++ or -- are not executed.

For the same reason you need to use HW semaphore even toggling bits in the same peripheral register, even if both cores are toggling different bits of the same register.

0 件の賞賛
返信