CAN Bus Timing (MCU : MC9S12XF512MLM)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN Bus Timing (MCU : MC9S12XF512MLM)

Jump to solution
4,517 Views
Kartoon67
Contributor III

Good afternoon,

 

I have some difficulties to configure CAN Bus Timing.

 

My clock source is configured at 4MHz. The configuration used in freescale example give me a CAN Bus Timing to 500kbp/s.

 

I would like to upgrade this speed to 1Mbit/s.

 

I try some example to modify Time Segment Values and prescaler, but it don't works for now.

 

That's why I required your help.

 

Best Regards,

 

 

 

Here the example of CAN Initilisation :

 

void vfnCAN_Init(void) {    CAN0CTL0 = 0x01;    /* MSCAN in initialization mode */        while (!(CAN0CTL1_INITAK))            ;         /* Wait for initialization mode acknowledge */                CAN0CTL1_CANE = 1;      /* Enable MSCAN module */    CAN0CTL1_CLKsrc=0;    /* Clock source is OSCCLK, CANCLK = 4MHz */        CAN0CTL1_LOOPB = 0;     /* Set to 1 for LoopBack Mode, 0 otherwise */    CAN0CTL1_LISTEN = 0;    /* Not listen only mode */                           /* Baud rate = CANCLK/(Prescaler * time quantas) */                                                                               CAN0BTR1_TSEG_10 = 0x04;    /* Time Segment 1 = 5 */    CAN0BTR1_TSEG_20 = 0x01;    /* Time Segment 2 = 2 */                                /* TSEG1 + TSEG2 + SYNCH_SEG = 8 time quantas */                                                                      /* Prescaler = CANCLK/(Baud rate * time quantas) = 4MHz/(500kHz * 8) = 1 */        CAN0BTR0_BRP = 0x00;    /* Baud rate prescaler = 1 */      CAN0BTR0_SJW = 0x01;    /* Sinchronization jump width = 2 clock cycles */                                      CAN0BTR1_SAMP = 0;      /* One sample per bit */                        CAN0IDAC_IDAM = 0x01;               /* Four 16-bit acceptance filters */                                                                  CAN0IDAR0 = 0xFF;                   /* 16 bit Filter 0 */    CAN0IDMR0 = 0xFF;                   /* No Filter */    CAN0IDAR1 = 0xFF;         CAN0IDMR1 = 0xFF;            CAN0IDAR2 = 0xFF;                   /* 16 bit Filter 1 */    CAN0IDMR2 = 0xFF;                   /* No Filter */    CAN0IDAR3 = 0xFF;                       CAN0IDMR3 = 0xFF;            CAN0IDAR4 = 0xFF;                   /* 16 bit Filter 2 */    CAN0IDMR4 = 0xFF;                   /* No Filter */    CAN0IDAR5 = 0xFF;                       CAN0IDMR5 = 0xFF;            CAN0IDAR6 = 0xFF;                   /* 16 bit Filter 3 */    CAN0IDMR6 = 0xFF;                   /* No Filter */    CAN0IDAR7 = 0xFF;                       CAN0IDMR7 = 0xFF;                CAN0CTL0 = 0x00;            /* Exit initialization mode request */        while (CAN0CTL1_INITAK)            ;                /* Wait for normal mode */                           while(!(CAN0CTL0_SYNCH))            ;                   /* Wait for CAN synchronization */       CAN0RFLG_RXF = 1;       /* Clear receiver flags */                                       CAN0RIER_RXFIE = 1;     /* Enable Full Receive Buffer interrupt */                                  }
Labels (1)
0 Kudos
Reply
1 Solution
4,020 Views
kef
Specialist I

Yes, you can use bus clock to clock CAN module. But you may either need to not enable PLL frequency modulation, or verify that resulting clock jitter won't disturb 1Mbps CAN bus. I'm not sure if this is a problem or not, I'm using higher oscilator clock for 1Mbps CAN.

If you are not sure about your settings, try creating experimental project with Processor Expert enabled, and see how it initializes peripherals.

View solution in original post

0 Kudos
Reply
5 Replies
4,020 Views
kef
Specialist I
  • My clock source is configured at 4MHz. The configuration used in freescale example give me a
  • CAN Bus Timing to 500kbp/s.
  • I would like to upgrade this speed to 1Mbit/s.

You can't . Your clock is to slow. But you may rise it probably using PLL.

0 Kudos
Reply
4,020 Views
Kartoon67
Contributor III

Hi,

 

And thanks for you reply.

 

The following parameter :

CAN0CTL1_CLKsrc=0;    /* Clock source is OSCCLK, CANCLK = 4MHz */

 can be configured  into CLOCK SOURCE or BUS CLOCK.

 

So, I know the bus clock do reference to the PLL generation. I generate an PLL of 40MHz like this :

 

void vfnClock_Settings(void){        /* Bus Clock = OSCCLK * (SYNR+1) / ((REFDV+1)(2*POSTDIV))    */    /*     40MHz =  4MHz  * (9+1) / (1)                          */    PLLCTL_PLLON = 0;       /* Disable the PLL */    SYNR_SYN = 0x09;        /* Set PLL synthesizer register to 9 */    REFDV_REFDV = 0x00;     /* Set PLL divider register to 0 */        /* Fvco = 2*OSCCLK*(SYNR+1)/(REFDV+1) = 8MHz* 10/1 = 80MHz   */    /*                                    -> VCOFRQ = 01b        */            SYNR_VCOFRQ1 = 0;    SYNR_VCOFRQ0 = 1;            /* Fref = OSCCLK/(REFDV+1) = 4MHz/1 = 4MHz -> REFRQ= 01b     */        REFDV_REFFRQ1 = 0;    REFDV_REFFRQ0 = 1;        PLLCTL_PLLON = 1;   /* PLL enabled */            while(!CRGFLG_LOCK)            ;       /* Wait until the PLL is within the desired frequency */                    CLKSEL_PLLSEL = 1;    /* Select clock source from PLL */      }

 

 So, i can use this bus clock to generate my CAN speed (1Mbit/s)?

 

Regards,

0 Kudos
Reply
4,021 Views
kef
Specialist I

Yes, you can use bus clock to clock CAN module. But you may either need to not enable PLL frequency modulation, or verify that resulting clock jitter won't disturb 1Mbps CAN bus. I'm not sure if this is a problem or not, I'm using higher oscilator clock for 1Mbps CAN.

If you are not sure about your settings, try creating experimental project with Processor Expert enabled, and see how it initializes peripherals.

0 Kudos
Reply
4,020 Views
Kartoon67
Contributor III

hi,

 

I try this and I think it works :

 

CAN0CTL1_CANE = 1;      /* Enable MSCAN module */    CAN0CTL1_CLKsrc=1;    /* Clock source is Bus CLOCK, CANCLK = 40MHz */        CAN0CTL1_LOOPB = 0;     /* Set to 1 for LoopBack Mode, 0 otherwise */    CAN0CTL1_LISTEN = 0;    /* Not listen only mode */                           /* Baud rate = CANCLK/(Prescaler * time quantas) */                                                                               CAN0BTR1_TSEG_10 = 0x0D;    /* Time Segment 1 = 14 */    CAN0BTR1_TSEG_20 = 0x04;    /* Time Segment 2 = 5 */                                /* TSEG1 + TSEG2 + SYNCH_SEG = 20 time quantas */                                                                      /* Prescaler = CANCLK/(Baud rate * time quantas) = 40MHz/(1MHz * 20) = 1 */        CAN0BTR0_BRP = 0x01;    /* Baud rate prescaler = 2 */      CAN0BTR0_SJW = 0x00;    /* Sinchronization jump width = 1 clock cycles */

 Now, my frames are sending at 1Mbit/s.

 

Regards

0 Kudos
Reply
4,020 Views
Kartoon67
Contributor III

I try this configuration :

 

    CAN0CTL1_CANE = 1;      /* Enable MSCAN module */    CAN0CTL1_CLKsrc=1;    /* Clock source is Bus CLOCK, CANCLK = 40MHz */        CAN0CTL1_LOOPB = 0;     /* Set to 1 for LoopBack Mode, 0 otherwise */    CAN0CTL1_LISTEN = 0;    /* Not listen only mode */                           /* Baud rate = CANCLK/(Prescaler * time quantas) */                                                                               CAN0BTR1_TSEG_10 = 0x04;    /* Time Segment 1 = 5 */    CAN0BTR1_TSEG_20 = 0x01;    /* Time Segment 2 = 2 */                                /* TSEG1 + TSEG2 + SYNCH_SEG = 8 time quantas */                                                                      /* Prescaler = CANCLK/(Baud rate * time quantas) = 40MHz/(8MHz * 8) = 5 */        CAN0BTR0_BRP = 0x05;    /* Baud rate prescaler = 5 */      CAN0BTR0_SJW = 0x01;    /* Sinchronization jump width = 2 clock cycles */                                 

 Am I right?

0 Kudos
Reply