CAN Bus Timing (MCU : MC9S12XF512MLM)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN Bus Timing (MCU : MC9S12XF512MLM)

ソリューションへジャンプ
4,448件の閲覧回数
Kartoon67
Contributor III

Good afternoon,

 

I have some difficulties to configure CAN Bus Timing.

 

My clock source is configured at 4MHz. The configuration used in freescale example give me a CAN Bus Timing to 500kbp/s.

 

I would like to upgrade this speed to 1Mbit/s.

 

I try some example to modify Time Segment Values and prescaler, but it don't works for now.

 

That's why I required your help.

 

Best Regards,

 

 

 

Here the example of CAN Initilisation :

 

void vfnCAN_Init(void) {    CAN0CTL0 = 0x01;    /* MSCAN in initialization mode */        while (!(CAN0CTL1_INITAK))            ;         /* Wait for initialization mode acknowledge */                CAN0CTL1_CANE = 1;      /* Enable MSCAN module */    CAN0CTL1_CLKsrc=0;    /* Clock source is OSCCLK, CANCLK = 4MHz */        CAN0CTL1_LOOPB = 0;     /* Set to 1 for LoopBack Mode, 0 otherwise */    CAN0CTL1_LISTEN = 0;    /* Not listen only mode */                           /* Baud rate = CANCLK/(Prescaler * time quantas) */                                                                               CAN0BTR1_TSEG_10 = 0x04;    /* Time Segment 1 = 5 */    CAN0BTR1_TSEG_20 = 0x01;    /* Time Segment 2 = 2 */                                /* TSEG1 + TSEG2 + SYNCH_SEG = 8 time quantas */                                                                      /* Prescaler = CANCLK/(Baud rate * time quantas) = 4MHz/(500kHz * 8) = 1 */        CAN0BTR0_BRP = 0x00;    /* Baud rate prescaler = 1 */      CAN0BTR0_SJW = 0x01;    /* Sinchronization jump width = 2 clock cycles */                                      CAN0BTR1_SAMP = 0;      /* One sample per bit */                        CAN0IDAC_IDAM = 0x01;               /* Four 16-bit acceptance filters */                                                                  CAN0IDAR0 = 0xFF;                   /* 16 bit Filter 0 */    CAN0IDMR0 = 0xFF;                   /* No Filter */    CAN0IDAR1 = 0xFF;         CAN0IDMR1 = 0xFF;            CAN0IDAR2 = 0xFF;                   /* 16 bit Filter 1 */    CAN0IDMR2 = 0xFF;                   /* No Filter */    CAN0IDAR3 = 0xFF;                       CAN0IDMR3 = 0xFF;            CAN0IDAR4 = 0xFF;                   /* 16 bit Filter 2 */    CAN0IDMR4 = 0xFF;                   /* No Filter */    CAN0IDAR5 = 0xFF;                       CAN0IDMR5 = 0xFF;            CAN0IDAR6 = 0xFF;                   /* 16 bit Filter 3 */    CAN0IDMR6 = 0xFF;                   /* No Filter */    CAN0IDAR7 = 0xFF;                       CAN0IDMR7 = 0xFF;                CAN0CTL0 = 0x00;            /* Exit initialization mode request */        while (CAN0CTL1_INITAK)            ;                /* Wait for normal mode */                           while(!(CAN0CTL0_SYNCH))            ;                   /* Wait for CAN synchronization */       CAN0RFLG_RXF = 1;       /* Clear receiver flags */                                       CAN0RIER_RXFIE = 1;     /* Enable Full Receive Buffer interrupt */                                  }
ラベル(1)
0 件の賞賛
返信
1 解決策
3,951件の閲覧回数
kef
Specialist I

Yes, you can use bus clock to clock CAN module. But you may either need to not enable PLL frequency modulation, or verify that resulting clock jitter won't disturb 1Mbps CAN bus. I'm not sure if this is a problem or not, I'm using higher oscilator clock for 1Mbps CAN.

If you are not sure about your settings, try creating experimental project with Processor Expert enabled, and see how it initializes peripherals.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,951件の閲覧回数
kef
Specialist I
  • My clock source is configured at 4MHz. The configuration used in freescale example give me a
  • CAN Bus Timing to 500kbp/s.
  • I would like to upgrade this speed to 1Mbit/s.

You can't . Your clock is to slow. But you may rise it probably using PLL.

0 件の賞賛
返信
3,951件の閲覧回数
Kartoon67
Contributor III

Hi,

 

And thanks for you reply.

 

The following parameter :

CAN0CTL1_CLKsrc=0;    /* Clock source is OSCCLK, CANCLK = 4MHz */

 can be configured  into CLOCK SOURCE or BUS CLOCK.

 

So, I know the bus clock do reference to the PLL generation. I generate an PLL of 40MHz like this :

 

void vfnClock_Settings(void){        /* Bus Clock = OSCCLK * (SYNR+1) / ((REFDV+1)(2*POSTDIV))    */    /*     40MHz =  4MHz  * (9+1) / (1)                          */    PLLCTL_PLLON = 0;       /* Disable the PLL */    SYNR_SYN = 0x09;        /* Set PLL synthesizer register to 9 */    REFDV_REFDV = 0x00;     /* Set PLL divider register to 0 */        /* Fvco = 2*OSCCLK*(SYNR+1)/(REFDV+1) = 8MHz* 10/1 = 80MHz   */    /*                                    -> VCOFRQ = 01b        */            SYNR_VCOFRQ1 = 0;    SYNR_VCOFRQ0 = 1;            /* Fref = OSCCLK/(REFDV+1) = 4MHz/1 = 4MHz -> REFRQ= 01b     */        REFDV_REFFRQ1 = 0;    REFDV_REFFRQ0 = 1;        PLLCTL_PLLON = 1;   /* PLL enabled */            while(!CRGFLG_LOCK)            ;       /* Wait until the PLL is within the desired frequency */                    CLKSEL_PLLSEL = 1;    /* Select clock source from PLL */      }

 

 So, i can use this bus clock to generate my CAN speed (1Mbit/s)?

 

Regards,

0 件の賞賛
返信
3,952件の閲覧回数
kef
Specialist I

Yes, you can use bus clock to clock CAN module. But you may either need to not enable PLL frequency modulation, or verify that resulting clock jitter won't disturb 1Mbps CAN bus. I'm not sure if this is a problem or not, I'm using higher oscilator clock for 1Mbps CAN.

If you are not sure about your settings, try creating experimental project with Processor Expert enabled, and see how it initializes peripherals.

0 件の賞賛
返信
3,951件の閲覧回数
Kartoon67
Contributor III

hi,

 

I try this and I think it works :

 

CAN0CTL1_CANE = 1;      /* Enable MSCAN module */    CAN0CTL1_CLKsrc=1;    /* Clock source is Bus CLOCK, CANCLK = 40MHz */        CAN0CTL1_LOOPB = 0;     /* Set to 1 for LoopBack Mode, 0 otherwise */    CAN0CTL1_LISTEN = 0;    /* Not listen only mode */                           /* Baud rate = CANCLK/(Prescaler * time quantas) */                                                                               CAN0BTR1_TSEG_10 = 0x0D;    /* Time Segment 1 = 14 */    CAN0BTR1_TSEG_20 = 0x04;    /* Time Segment 2 = 5 */                                /* TSEG1 + TSEG2 + SYNCH_SEG = 20 time quantas */                                                                      /* Prescaler = CANCLK/(Baud rate * time quantas) = 40MHz/(1MHz * 20) = 1 */        CAN0BTR0_BRP = 0x01;    /* Baud rate prescaler = 2 */      CAN0BTR0_SJW = 0x00;    /* Sinchronization jump width = 1 clock cycles */

 Now, my frames are sending at 1Mbit/s.

 

Regards

0 件の賞賛
返信
3,951件の閲覧回数
Kartoon67
Contributor III

I try this configuration :

 

    CAN0CTL1_CANE = 1;      /* Enable MSCAN module */    CAN0CTL1_CLKsrc=1;    /* Clock source is Bus CLOCK, CANCLK = 40MHz */        CAN0CTL1_LOOPB = 0;     /* Set to 1 for LoopBack Mode, 0 otherwise */    CAN0CTL1_LISTEN = 0;    /* Not listen only mode */                           /* Baud rate = CANCLK/(Prescaler * time quantas) */                                                                               CAN0BTR1_TSEG_10 = 0x04;    /* Time Segment 1 = 5 */    CAN0BTR1_TSEG_20 = 0x01;    /* Time Segment 2 = 2 */                                /* TSEG1 + TSEG2 + SYNCH_SEG = 8 time quantas */                                                                      /* Prescaler = CANCLK/(Baud rate * time quantas) = 40MHz/(8MHz * 8) = 5 */        CAN0BTR0_BRP = 0x05;    /* Baud rate prescaler = 5 */      CAN0BTR0_SJW = 0x01;    /* Sinchronization jump width = 2 clock cycles */                                 

 Am I right?

0 件の賞賛
返信