C++ Compilers?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

C++ Compilers?

2,106 Views
bubba
Contributor I
Is there a C++ compiler for the 56F8367 DSP or any of the other Freescale DSPs?
Could anyone recommend a C++ compiler for the 56F8367?
 
This is a CodeWarrior house; however, I would like to know what options are out there.  Also if there are no C++ compilers for the DSPs...
 
Could anyone recommend a processor that does have a C++ compiler with similar pricing and features to the 56F8367 DSP?  (NOTE:  We don't generally use the extra DSP instructions.)
 
Thanks!
 
Labels (1)
0 Kudos
Reply
1 Reply

1,189 Views
muelland
Contributor I
I'm in the same boat as bubba.

I am evaluating the MC56F8357 for a large project at my company but require a c++ compiler. Codewarrior for the 56F8300 family only supports C (per the documentation). Having to use C instead of C++ will have a large negative effect our time line.

Is there an alternative c++ compiler to use for this chip or are we stuck with C and Codewarrior?
0 Kudos
Reply