Build Error for MC9S12ZVML128_LIN_BLDC_Sensorless using CodeWarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Build Error for MC9S12ZVML128_LIN_BLDC_Sensorless using CodeWarrior

跳至解决方案
2,398 次查看
itsnewforme
Contributor IV

I'm trying to build the code MC9S12ZVML128_LIN_BLDC_Sensorless using CodeWarrior IDE. It is giving me the following errors. How to resolve them ?

Description Resource Path Location Type
mingw32-make: *** [src/S12ZVM_system/vector_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_common_proto_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/S12ZVM_system/startup_CW/startup_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/S12ZVM_system/startup_CW/mc9s12zvml128_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/lowlevel/lin_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_common_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/transport/lin_commontl_proto_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_j2602_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
Invalid project path: Include path not found (C:\Freescale\CW MCU v10.7\MCU\S12lisa_Support\s12lisac\src). MC9S12ZVML128_LIN_BLDC_Sensorless pathentry Path Entry Problem
Invalid project path: Include path not found (C:\Freescale\CW MCU v10.7\MCU\S12lisa_Support\s12lisac\lib_small). MC9S12ZVML128_LIN_BLDC_Sensorless pathentry Path Entry Problem
Invalid project path: Include path not found (C:\Freescale\AMMCLIB\MC9S12ZVM_AMMCLIB_v1.0.2\include). MC9S12ZVML128_LIN_BLDC_Sensorless pathentry Path Entry Problem
Invalid project path: Include path not found (C:\Freescale\CW MCU v10.7\MCU\S12lisa_Support\s12lisac\include). MC9S12ZVML128_LIN_BLDC_Sensorless pathentry Path Entry Problem
mingw32-make: *** [MC9S12ZVML128_BLDC_Sensorless_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** Waiting for unfinished jobs.... MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/diagnostic/lin_diagnostic_service_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/transport/lin_j2602tl_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/transport/lin_lin21tl_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_j2602_proto_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_lin21_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_lin21_proto_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/transport/lin_commontl_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem

0 项奖励
回复
1 解答
2,387 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @itsnewforme,

Which version of the demo SW do you use?

You should find release notes in the installation directory, it specifies compatible CW revisions.

Also, when you download the latest version of the SW, you should use it with the latest Automotive Math and Motor Control Library (AMMCLIB).

 

Regards,

Daniel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,388 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @itsnewforme,

Which version of the demo SW do you use?

You should find release notes in the installation directory, it specifies compatible CW revisions.

Also, when you download the latest version of the SW, you should use it with the latest Automotive Math and Motor Control Library (AMMCLIB).

 

Regards,

Daniel

0 项奖励
回复
2,381 次查看
itsnewforme
Contributor IV

Yes, It was a library issue. Thanks for helping :))

0 项奖励
回复