Build Error for MC9S12ZVML128_LIN_BLDC_Sensorless using CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build Error for MC9S12ZVML128_LIN_BLDC_Sensorless using CodeWarrior

ソリューションへジャンプ
2,327件の閲覧回数
itsnewforme
Contributor IV

I'm trying to build the code MC9S12ZVML128_LIN_BLDC_Sensorless using CodeWarrior IDE. It is giving me the following errors. How to resolve them ?

Description Resource Path Location Type
mingw32-make: *** [src/S12ZVM_system/vector_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_common_proto_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/S12ZVM_system/startup_CW/startup_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/S12ZVM_system/startup_CW/mc9s12zvml128_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/lowlevel/lin_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_common_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/transport/lin_commontl_proto_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_j2602_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
Invalid project path: Include path not found (C:\Freescale\CW MCU v10.7\MCU\S12lisa_Support\s12lisac\src). MC9S12ZVML128_LIN_BLDC_Sensorless pathentry Path Entry Problem
Invalid project path: Include path not found (C:\Freescale\CW MCU v10.7\MCU\S12lisa_Support\s12lisac\lib_small). MC9S12ZVML128_LIN_BLDC_Sensorless pathentry Path Entry Problem
Invalid project path: Include path not found (C:\Freescale\AMMCLIB\MC9S12ZVM_AMMCLIB_v1.0.2\include). MC9S12ZVML128_LIN_BLDC_Sensorless pathentry Path Entry Problem
Invalid project path: Include path not found (C:\Freescale\CW MCU v10.7\MCU\S12lisa_Support\s12lisac\include). MC9S12ZVML128_LIN_BLDC_Sensorless pathentry Path Entry Problem
mingw32-make: *** [MC9S12ZVML128_BLDC_Sensorless_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** Waiting for unfinished jobs.... MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/diagnostic/lin_diagnostic_service_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/transport/lin_j2602tl_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/transport/lin_lin21tl_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_j2602_proto_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_lin21_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/coreapi/lin_lin21_proto_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem
mingw32-make: *** [src/LIN/LIN_driver/transport/lin_commontl_api_c.obj] Error 1 MC9S12ZVML128_LIN_BLDC_Sensorless C/C++ Problem

0 件の賞賛
返信
1 解決策
2,316件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @itsnewforme,

Which version of the demo SW do you use?

You should find release notes in the installation directory, it specifies compatible CW revisions.

Also, when you download the latest version of the SW, you should use it with the latest Automotive Math and Motor Control Library (AMMCLIB).

 

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,317件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @itsnewforme,

Which version of the demo SW do you use?

You should find release notes in the installation directory, it specifies compatible CW revisions.

Also, when you download the latest version of the SW, you should use it with the latest Automotive Math and Motor Control Library (AMMCLIB).

 

Regards,

Daniel

0 件の賞賛
返信
2,310件の閲覧回数
itsnewforme
Contributor IV

Yes, It was a library issue. Thanks for helping :))

0 件の賞賛
返信