Bootloader for NE64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader for NE64

2,219 Views
IamX
Contributor I
Hi
I develop NE64_OpenTCP with CodeWarrior+P&E ICD Programming.
Finaly.I want to update firmware without P&E ICD Programming.
Which way for do it.?
if use bootloader.How to use bootloader for programming NE_Opentcp via RS-232 .
Thank you for advantage
Mr.X
 

 
Labels (1)
0 Kudos
Reply
1 Reply

1,246 Views
mjbcswitzerland
Specialist V
Hi Mr X

If you have the Freescale Serial Monitor installed in your NE64 then you can upload SREC files via SCI0.

The serial monitor can be loaded using P&E (if not already loaded) or using a DEMOS12NE64. See the following link sfor a software to load to the DEMOS12NE64 (or other boards) to convert it to a BDM and also a free serial loading software:

http://www.utasker.com/docs/documentation.html (see "Guide to converting a DEMO9S12NE64 into a LAN based BDM programming tool for the MC9S12NE64 )

http://www.utasker.com/software/software.html (see "A download utility for programming DEMO9S12NE64 via serial port with basic debugging support as well )

Regards

0 Kudos
Reply