Bootloader ,Using SRecCvt-GUI to convert S19 file ,No output??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader ,Using SRecCvt-GUI to convert S19 file ,No output??

1,516 Views
ChenBowen
Contributor II

I just want to use the SRecCvt-GUI to convert the Project.abs.s19 file for CAN-BootLoader(xs128) using.But when I do like the follow

ChenBowen_0-1641049731937.pngChenBowen_0-1641049731937.png

Why no output?  Why the Debug mode says "Can't Open Input File "?

0 Kudos
Reply
1 Reply

1,498 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

I am not able to test it because of your folder structure. However, what I suggest is to copy the original S19 file into the SRecCvt folder and convert it there. It is better to use "no path" access to avoid any problems with tree structure.

Best regards,

Ladislav

0 Kudos
Reply