Bootloader ,Using SRecCvt-GUI to convert S19 file ,No output??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader ,Using SRecCvt-GUI to convert S19 file ,No output??

1,545件の閲覧回数
ChenBowen
Contributor II

I just want to use the SRecCvt-GUI to convert the Project.abs.s19 file for CAN-BootLoader(xs128) using.But when I do like the follow

ChenBowen_0-1641049731937.png

Why no output?  Why the Debug mode says "Can't Open Input File "?

0 件の賞賛
返信
1 返信

1,527件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

I am not able to test it because of your folder structure. However, what I suggest is to copy the original S19 file into the SRecCvt folder and convert it there. It is better to use "no path" access to avoid any problems with tree structure.

Best regards,

Ladislav

0 件の賞賛
返信