BLDC Motors param

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLDC Motors param

Jump to solution
2,377 Views
sufree
Contributor II

Hello,

I reference the document AN4704 and code to  do research of Sensorless Control of BLDC Motors use MC9S12ZVM .And in the code as follow:  

I do not know: why SPEED_CALC_NUMERATOR=16777216?  1431.655765 = 1000 rpm? How to calculation it ?

 Thanks!

#ifdef _HIGH_SPEED_SCALING
/***** High speed scaling *********************
* For 4 pole-pairs motors
* Boundary values for 1.28 us timer period:
* - Minimal speed: 60 rpm
* - Minimal speed scaled: 86
* - Maximal speed: 22887 rpm
* - Maximal speed scaled: 32767
*********************************************/
#define SPEED_CALC_NUMERATOR 16777216
#define STALLCHECK_MIN_CMT_PERIOD 97 // 97 = 125 us (20 krpm on 4 pole-pairs motor), min value = 85 (22.89 krpm)
#define REQUIRED_RUN_SPEED 1432 //   1431.655765 = 1000 rpm
#define MIN_SPEED (1432/2) // 500 rpm minimal speed for Down button control (should be min 10% of nominal motor speed)
#define MAX_SPEED (1432*13) // 13 krpm maximum speed for Up button control
#define SPEED_STEP (1432/2) // 500 rpm, Up/Down step for button controls
//*****
#endif

period6ZC = periodZC_F_PhA + periodZC_R_PhA + periodZC_F_PhB + periodZC_R_PhB + periodZC_F_PhC + periodZC_R_PhC;
actualSpeed = SPEED_CALC_NUMERATOR / period6ZC;

0 Kudos
Reply
1 Solution
2,216 Views
pachamatej
NXP Employee
NXP Employee

Hi,

The numbers make the connection between the commutation time and speed in terms of Timer ticks.

If the floating point representation is used, it's agreed that the math between speed and commutation period is given:

Speed_RPS = 1 / (CommutationPeriod * PolePairs)

CommutationPeriod = 1 / (Speed_RPS * PolePairs)

Speed_RPS = Speed_RPM / 60

In 1.15 fractional implementation <-1.0, 1.0), the situation is scaled to a "numerator", which helps the calculation to stay within the scale, considering integer type casting.

tFrac16_Speed = tU32_Numerator / (tU16_CommutationPeriod * tU16_PolePairs)

tU16_CommutationPeriod = tU32_Numerator / (tFrac16_Speed * tU16_PolePairs)

While we typically use higher pole-paired motors, the numerator should be calculated based on the pole-pairs.

Some advanced math behind:

We can start with the maximal speed, let's say MaxSpeed = 15000 RPM and PolePairs = 4. That means, the CommutationPeriod = 1 / (15000/60 * 4) = 1 ms

Let's set the minimum number of timer ticks per one commutation, which gives us a precission of the commutation:

MinTicksPerCommutation = 512

Now, our system uses 1.15 fraction format, which means the maximum integer number is ideally 32768. This gives us the base for our Numerator:

tU32_Numerator = MinTicksPerCommutation * 32768 = 16777216

With the minimal CommutationPeriod = 0.5 ms and MinTicksPerCommutation = 512, we can calculate the timer domain:

MaxTickTime = MinCommutationPeriod / MinTicksPerCommutation = 1.9... us. Now, the fBus divider is calculated, based on the fBus = 50 MHz

TimerDivider ~ MaxTickTime * fBus = 96., thus nearest TimerDivider = 64

TimerTickFrequency = fBus / TimerDivider = 781.25 kHz

TickTime = 1.28 us

 

Since we have selected a different TimerDivider, the scale is slightly different for corner case:

MinCommutationPeriod = TickTime * MinTicksPerCommutation = 1.28us * 512 = 0,655 ms

MaxSpeed = 1 / (MinCommutationPeriod / 60 * 4) = 22 900

In the example, the speed is calculated simply by adding all the commutation periods and recalculating using the formula above.

For the speed scale, just consider following:

tFrac16 maximum is 32767

MaxSpeed is 22900

If the required speed is 1000 RPM, its integer representation is then 32768 / 22900 * 1000 RPM = 1431 RPM

I hope it will help.

Best regards,

Matej

View solution in original post

0 Kudos
Reply
2 Replies
2,217 Views
pachamatej
NXP Employee
NXP Employee

Hi,

The numbers make the connection between the commutation time and speed in terms of Timer ticks.

If the floating point representation is used, it's agreed that the math between speed and commutation period is given:

Speed_RPS = 1 / (CommutationPeriod * PolePairs)

CommutationPeriod = 1 / (Speed_RPS * PolePairs)

Speed_RPS = Speed_RPM / 60

In 1.15 fractional implementation <-1.0, 1.0), the situation is scaled to a "numerator", which helps the calculation to stay within the scale, considering integer type casting.

tFrac16_Speed = tU32_Numerator / (tU16_CommutationPeriod * tU16_PolePairs)

tU16_CommutationPeriod = tU32_Numerator / (tFrac16_Speed * tU16_PolePairs)

While we typically use higher pole-paired motors, the numerator should be calculated based on the pole-pairs.

Some advanced math behind:

We can start with the maximal speed, let's say MaxSpeed = 15000 RPM and PolePairs = 4. That means, the CommutationPeriod = 1 / (15000/60 * 4) = 1 ms

Let's set the minimum number of timer ticks per one commutation, which gives us a precission of the commutation:

MinTicksPerCommutation = 512

Now, our system uses 1.15 fraction format, which means the maximum integer number is ideally 32768. This gives us the base for our Numerator:

tU32_Numerator = MinTicksPerCommutation * 32768 = 16777216

With the minimal CommutationPeriod = 0.5 ms and MinTicksPerCommutation = 512, we can calculate the timer domain:

MaxTickTime = MinCommutationPeriod / MinTicksPerCommutation = 1.9... us. Now, the fBus divider is calculated, based on the fBus = 50 MHz

TimerDivider ~ MaxTickTime * fBus = 96., thus nearest TimerDivider = 64

TimerTickFrequency = fBus / TimerDivider = 781.25 kHz

TickTime = 1.28 us

 

Since we have selected a different TimerDivider, the scale is slightly different for corner case:

MinCommutationPeriod = TickTime * MinTicksPerCommutation = 1.28us * 512 = 0,655 ms

MaxSpeed = 1 / (MinCommutationPeriod / 60 * 4) = 22 900

In the example, the speed is calculated simply by adding all the commutation periods and recalculating using the formula above.

For the speed scale, just consider following:

tFrac16 maximum is 32767

MaxSpeed is 22900

If the required speed is 1000 RPM, its integer representation is then 32768 / 22900 * 1000 RPM = 1431 RPM

I hope it will help.

Best regards,

Matej

0 Kudos
Reply
2,216 Views
sufree
Contributor II

Hello  Matej,

Thank you very much!

0 Kudos
Reply