Array over 123 elements

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Array over 123 elements

ソリューションへジャンプ
2,475件の閲覧回数
aaronlee
Contributor V

Hi,

My project is using S12ZVCA. I have an issue about array over 123 element as follow:

void main(void) {
const unsigned int TemperatureTable[124]={ 
4924, 4920, 4915, 4910, 4905, 4900, 4894, 4888, 4882, 4876,
4869, 4862, 4855, 4847, 4839, 4831, 4822, 4813, 4803, 4794,
4783, 4773, 4761, 4750, 4738, 4725, 4712, 4699, 4685, 4671,
4656, 4640, 4624, 4608, 4590, 4573, 4555, 4536, 4516, 4496,
4476,
4454, 4432, 4410, 4387, 4363, 4338, 4314, 4288, 4262, 4235,
4207, 4179, 4150, 4121, 4091, 4060, 4029, 3998, 3965, 3933,
3899, 3864, 3830, 3795, 3759, 3723, 3687, 3650, 3612, 3575,
3536, 3498, 3459, 3420, 3380, 3340, 3300, 3260, 3219, 3178,
3137, 3096, 3055, 3014, 2973, 2931, 2890, 2849, 2807, 2766,
2725, 2684, 2643, 2602, 2562, 2521, 2481, 2441, 2401, 2362,
2322, 2284, 2245, 2207, 2169, 2131, 2094, 2057, 2021, 1985,
1949, 1914, 1879, 1845, 1810, 1777, 1744, 1711, 1679, 1648,
1617, 1586, 1555};

}

I execute step by step in debugging mode. It terminate after assign array TemperatureTable[124]={......}.

Then show message as follow:

No source available for "0x0001F1 (0x0001F1)() "

It can work when elements of array less than 123. How to resolve the issue?

Best Regards,

Aaron

タグ(2)
1 解決策
2,173件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The reason for this is that the array is placed on the stack.

So you can extend the stacksize in the linker file:

 stack.png

You can place the array as global (before the main function), or declare it as a static array.

Also, there is an article S12Z constant, variable, code allocation in CodeWarrior you can refer to.

Regards,

Daniel

元の投稿で解決策を見る

1 返信
2,173件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The reason for this is that the array is placed on the stack.

So you can extend the stacksize in the linker file:

 stack.png

You can place the array as global (before the main function), or declare it as a static array.

Also, there is an article S12Z constant, variable, code allocation in CodeWarrior you can refer to.

Regards,

Daniel