Array over 123 elements

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Array over 123 elements

Jump to solution
2,353 Views
aaronlee
Contributor V

Hi,

My project is using S12ZVCA. I have an issue about array over 123 element as follow:

void main(void) {
const unsigned int TemperatureTable[124]={ 
4924, 4920, 4915, 4910, 4905, 4900, 4894, 4888, 4882, 4876,
4869, 4862, 4855, 4847, 4839, 4831, 4822, 4813, 4803, 4794,
4783, 4773, 4761, 4750, 4738, 4725, 4712, 4699, 4685, 4671,
4656, 4640, 4624, 4608, 4590, 4573, 4555, 4536, 4516, 4496,
4476,
4454, 4432, 4410, 4387, 4363, 4338, 4314, 4288, 4262, 4235,
4207, 4179, 4150, 4121, 4091, 4060, 4029, 3998, 3965, 3933,
3899, 3864, 3830, 3795, 3759, 3723, 3687, 3650, 3612, 3575,
3536, 3498, 3459, 3420, 3380, 3340, 3300, 3260, 3219, 3178,
3137, 3096, 3055, 3014, 2973, 2931, 2890, 2849, 2807, 2766,
2725, 2684, 2643, 2602, 2562, 2521, 2481, 2441, 2401, 2362,
2322, 2284, 2245, 2207, 2169, 2131, 2094, 2057, 2021, 1985,
1949, 1914, 1879, 1845, 1810, 1777, 1744, 1711, 1679, 1648,
1617, 1586, 1555};

}

I execute step by step in debugging mode. It terminate after assign array TemperatureTable[124]={......}.

Then show message as follow:

No source available for "0x0001F1 (0x0001F1)() "

It can work when elements of array less than 123. How to resolve the issue?

Best Regards,

Aaron

1 Solution
2,051 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The reason for this is that the array is placed on the stack.

So you can extend the stacksize in the linker file:

 stack.png

You can place the array as global (before the main function), or declare it as a static array.

Also, there is an article S12Z constant, variable, code allocation in CodeWarrior you can refer to.

Regards,

Daniel

View solution in original post

1 Reply
2,052 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The reason for this is that the array is placed on the stack.

So you can extend the stacksize in the linker file:

 stack.png

You can place the array as global (before the main function), or declare it as a static array.

Also, there is an article S12Z constant, variable, code allocation in CodeWarrior you can refer to.

Regards,

Daniel