About programming type (OSBDM ? Writer ?)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About programming type (OSBDM ? Writer ?)

3,610件の閲覧回数
miles
Contributor I

Dear Sir:

I study S12ZVC and has some question :
1. What are the ways to burn program? Is it possible to provide hardware or technical documentation for reference?
2. Does OSBDM also burn or buy writer? Can provide OSBDM code and documentation for burn program demand

Please assist for my question, TKS !

6 返答(返信)

2,954件の閲覧回数
aaronlee
Contributor V

Hi,

I buy the new notebook. O.S. is windows 10.

I install the following software

  • CodeWarrior for MCU Version: 10.7 Build Id:160721
  • multilink_universal_install

The Multilink Universal can not work with my new notebook.

pastedImage_2.png

The Device manager as following:

pastedImage_3.png

I try many way, but the issue still here. Any recommend?

Best Regards,

Aaron

0 件の賞賛
返信

2,954件の閲覧回数
aaronlee
Contributor V

Hi,

I resolved the problem.

FAQ Link: PEmicro FAQ 

Driver download:  P&E Hardware Interface Drivers, Version 12 (Win XP/Vista/7/8/10) 

Best Regards,

Aaron

0 件の賞賛
返信

2,954件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello

The MCU has BDC/BDG module and support USB multilink. You can use OSBDM to burn/debug as well.

The NXP S12Z boards use OSBDM interface MC9S08JM60: Datasheet, AN3561 USB Bootloader for the MC9S08JM60, schematic. Refer to PEmicro for source code and more information.

 

You can flash the MCU using CodeWarrior, the Special Edition of which is free-download, fully functional tool with only code size restrictions on the build chain. So, once you have built the code, you can use it to flash the MCU regardless of the code size.

Regards

Daniel

0 件の賞賛
返信

2,954件の閲覧回数
aaronlee
Contributor V

Hi,

I plan to use S12ZVCA and flash it by DBC/DBG module.

What can  I  buy the DBC/DBG programmer ?

Is the S12ZVC MCU build-in any bootloader ?

May I use AN4258, Serial Bootloader for S12(X) Microcontrollers Based on 180 nm Techno ... in S12ZVCA ?

Regards,

Aaron

0 件の賞賛
返信

2,954件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi

 

The product website recommends Software and tools.

We use PEmicro. The AN4258 bootloader is only for S12(X).

There is AN4723 for S12Z MagniV Bootloader: AN4723_SW.zip

 

Regards

Daniel

2,954件の閲覧回数
aaronlee
Contributor V

I buy the PEmicro Multilink Universal. It work well with 6-Pin BDM of DEVKIT-S12ZVC. Thank you.

0 件の賞賛
返信