AN2720 Files for Codewarrior stationery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN2720 Files for Codewarrior stationery

2,446 Views
colinh
Contributor I
Hi

Just trying to track down some source for AN2720 which has been updated for Codewarrior stationery.  I have some "hacked" stuff but have lost track of the originals.  The header for FLASH.C is

Code:
/******************************************************************* *                    freescale semiconductor inc  * *    DESCRIPTION:   S12 single array Flash routines *    SOURCE:        flash.c *    COPYRIGHT:     © 04/2004   freescale *    AUTHOR:        rat579  *    REV. HISTORY:  09/2004   - Added support for multiple array devices *          - Modified for MW standard stationery. * * *******************************************************************/

 The AN2720SW files currently on the website do not include the revs listed above.

Any help appreciated.

Thanks
Colin

PS: Is rat579 out there?

Labels (1)
0 Kudos
Reply
2 Replies

1,298 Views
JimDon
Senior Contributor III
If you do a Keyword search on AN2720 you should get two an2720sw.zip file hits.
One of them is the new one.
(one is like 83K the other, new one is 694K and has a complete CW project in it).
0 Kudos
Reply

1,298 Views
colinh
Contributor I
Thanks Jim

I have a few concerns about the code in the CW version - (but it could just be too many late nights playing tricks) I'll have a closer look and might follow this up on the forum a bit later.

Cheers
Colin
0 Kudos
Reply