AN2720 Files for Codewarrior stationery

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN2720 Files for Codewarrior stationery

2,459件の閲覧回数
colinh
Contributor I
Hi

Just trying to track down some source for AN2720 which has been updated for Codewarrior stationery.  I have some "hacked" stuff but have lost track of the originals.  The header for FLASH.C is

Code:
/******************************************************************* *                    freescale semiconductor inc  * *    DESCRIPTION:   S12 single array Flash routines *    SOURCE:        flash.c *    COPYRIGHT:     © 04/2004   freescale *    AUTHOR:        rat579  *    REV. HISTORY:  09/2004   - Added support for multiple array devices *          - Modified for MW standard stationery. * * *******************************************************************/

 The AN2720SW files currently on the website do not include the revs listed above.

Any help appreciated.

Thanks
Colin

PS: Is rat579 out there?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,311件の閲覧回数
JimDon
Senior Contributor III
If you do a Keyword search on AN2720 you should get two an2720sw.zip file hits.
One of them is the new one.
(one is like 83K the other, new one is 694K and has a complete CW project in it).
0 件の賞賛
返信

1,311件の閲覧回数
colinh
Contributor I
Thanks Jim

I have a few concerns about the code in the CW version - (but it could just be too many late nights playing tricks) I'll have a closer look and might follow this up on the forum a bit later.

Cheers
Colin
0 件の賞賛
返信