ADC - external trigger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC - external trigger

3,314 Views
gavryus
Contributor I
Hello,
 
I use for developement an S12XDP512 board and I need to use the external trigger for ADC.
 
My question is: ATDCTL2.ETRIGLE = 1 and ATDCTL2.ETRIGP = 0 (low level) means that as long as the external trigger signal is low (0 logic) the conversion is triggered?
 
Thank you!
Labels (1)
0 Kudos
Reply
2 Replies

1,717 Views
gavryus
Contributor I
 
Thank you for your help, Danny!
0 Kudos
Reply

1,717 Views
DannyM83
Contributor III
Yes, that is correct. You should also ensure that External Trigger Mode is enabled (ATDCTL2.ETRIGE = 1) and that the port to which the trigger is attached is entered to ATDCTL1.

Hope that helps,

Danny
0 Kudos
Reply