Thank you for your reply.
But unfortunately, I don't think I understood because I have little development experience.
The intention of my initial question was not to enter BOOT mode through a physical method such as an external switch.
The question was whether it could be controlled solely through S/W, excluding switches or separate H/W methods.
Do the examples or methods you answered fit the intent of my question?
Also, I didn't understand the following explanation.
(Note, the COP is not debugable because during reset the MCU lost connection with the IDE.)
I am currently working with Code Warrior (IDE) by connecting to the MCU on the development board via P&E USB multilink.
1. Does this explanation mean that if COP is reset while monitoring through IDE by connecting MCU and P&E, debugging is impossible because the connection between MCU and IDE is disconnected?
or not
2. Assuming that the P&E debugger is not connected...
In other words, does this mean that the COP of the written source code cannot be reset when the product is turned on, as in the development completion stage?
If the second is correct, it probably won't happen because you'll have to add a switch eventually, but I'm asking just to confirm.
Thank you Ladislav.