40 DIP Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

40 DIP Microcontroller

3,030 Views
wärmekältetechn
Contributor I

Hi guys i'm looking for Motorola 40 DIP Microcontroller  1F15b  CTCTAB9831 need any halp .thanks

Labels (1)
0 Kudos
Reply
5 Replies

2,863 Views
wärmekältetechn
Contributor I

ok thank you iggi i would try to copy the ic with GoodFET

0 Kudos
Reply

2,863 Views
wärmekältetechn
Contributor I

Hi iggi thank you i ask freescale but i don't get information (customer specific ic only customer can get information) over Motorola Logo can reading ECO STC-1.3 (eco german electronic manufacturer) 915.012 .

regards sascha

0 Kudos
Reply

2,863 Views
iggi
NXP Employee
NXP Employee

This seems to be some old HC05 or HC11 part. Don't you have the exact part number?

The characters you provided are maskset and LOT code which does not help much.

Still, HC05 and HC11 are obsolete products. You would need to look for the part at distributors.

Regards,

iggi

0 Kudos
Reply

2,863 Views
wärmekältetechn
Contributor I

Hi iggi if it's 68000 family wath programming interface can i take to read program from ic?

0 Kudos
Reply

2,863 Views
iggi
NXP Employee
NXP Employee

If you've been told the device is customer specific, then i'm afraid i can't help you more.
It looks like you might want to hack the micro :-)

The 68000 series are MPUs which means no flash on chip. And also this series you want find in 40-pin DIP package.

0 Kudos
Reply