Pearing NXP rapid IoT with windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pearing NXP rapid IoT with windows

3,708 Views
mdobrea
Contributor I

Hi to everyone !!

I wrote this question because I have a problem. I wish to pair a NXP rapid IoT with a Windows operating system.

When I go to the Bluetooth & other devices -> Add Bluetooth or other devices -> on Add device panel I am able to "see" the NXP rapid IoT, but when I tray to connect I receive the following error: "Try connecting your device again".

Any ideas or information?

Thanks very much !

Labels (1)
0 Kudos
Reply
8 Replies

3,303 Views
europevideo
Contributor II

Hi,

Same problem here, same error.

Hans

0 Kudos
Reply

3,303 Views
mdobrea
Contributor I

I have 2 different NXP rapid IoT and both have the same behavior (counting also the device belonging to Jose Manuel Cano Garcia, there a three with the same problem): it is impossible to pair them with the Windows, using the interface and tools provided by Microsoft.
Best regards,

                 Dan Dobrea.

0 Kudos
Reply

3,303 Views
josemanuelcanog
Contributor I

Hi Estephania, 

Thank you for replying.

Yes you are right; I have developped my own application using the Qt framework, It works  OK in linux, but not in windows (I get the same message shown/reported above). I have also tried other third-party tools in linux (such as the command line tools gatttool and bluetoothctl and both work fine, I am able to connect to the device, search services, read/write characteristics, activate characteristics notification, etc.). But in windows, when trying to add the device using the windows system control panel (windows native "add bluetooth device" menu, outside my application) it also fails with the same error, so I think it is not a problem specific to my application.

I developped a similar application for testing some of the examples of the FRDM-KW41Z (health thermometer,  heartrate, etc), and all of them worked fine both  for linux and windows computers. The characteristics and services are diferent in the rapid IoT kit, of course, but my custom application is essentially the same (connects to devices, search  services and tries to enable notification for some characteristics). For the FRDM-KW41Z it works fine. but for the rapid iot kit it fails when trying to connect (after a while the message above is shown),

Again, manually adding the FRDM-KW41Z through the windows "add bluetooth device" menu (outside my app) works fine for FRDM-KW41Z, but fails for rapid iot kit (again the same behaviour, the error message shown above is displayed). That is why I was wondering if someone has managed to connect the device to a windows computer (with either a custom or a third party app).

I tried changing some parameters of the rapid iot device firmware (particularly those related with pairing/bonding), but no sucess so far.

Best Regards,

Jose

0 Kudos
Reply

3,303 Views
mdobrea
Contributor I

Yes I'm using Rapid IoT Kit Out Of Box Demo. The windows (Version 1803 - OS Build 17134.590) detect the device (Rapid IoT) see below - B22F are the last characters of the number printed on the back of the case. But when I want to connect, each time I get this error:

Capture.PNG

I imagine that the problem is related to the Bluetooth communication parameters. So in the studio I change the BLEConnection block parameters to "Custom Passkey" and "Just Works" (in PAIRING TYPE field) - Random Passkey it was initially. I got the same error.

Are there other places to change the Bluetooth communication parameters ? Or do you have other solutions ?

Thanks a lot !

              Dobrea Dan.

0 Kudos
Reply

3,303 Views
josemanuelcanog
Contributor I

Hi,

I have the same problem.

I have written a Qt application that connects to the rapid IoT device and it works OK for Linux. Oher linux command-line tools such as gatttool and bluetoothctl can connect to the device, too.

But in windows, my Qt app does not connect successfully to the device, neither am I able to pair the computer with the device using the windows standard "add bluetooth device" dialog. It fails and displays the same message displayed above.

Has anyone managed to pair the rapid iot device with windows 10?

Regards,

Jose

0 Kudos
Reply

3,303 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

just to fully understand your problem, it does pairs in Linux but not in Windows? Is that correct? Also, you are pairing it with your own application, right?   

Regards, 

Estephania 

0 Kudos
Reply

3,303 Views
josemanuelcanog
Contributor I

Hi again, Estephania,

Any suggestion/pointer on this issue so far? I know  windows have some limitations supporting bluetooth, but it works perfecly with FRDM-KW41Z whereas It won't connect to the rapid IoT kit. Maybe it is necessary to update the firmware of the KW41Z subsystem embbedded in the rapid IoT kit?

Regards,

Jose

0 Kudos
Reply

3,303 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Are you working with the Out of the Box example in the Rapid IoT ? 

Regards, 
Estephania

0 Kudos
Reply