How to reset Rapid IoT after multiple pairing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to reset Rapid IoT after multiple pairing

ソリューションへジャンプ
3,273件の閲覧回数
cswiger
Contributor II

Looks like I made a mistake of pairing the Rapid IoT device with a phone (worked find), then deleting and pairing it with a tablet (worked fine), and now trying to go back to the phone.  At this point neither can pair with the device - actually they START to, either will find it, provision, the device even DISPLAY THE CORRECT TIME briefly then resets and is never seen again. Have tried many times since with no luck, let battery drain, etc. 

So the question is - how to reset it so I can pair with one phone and leave it there?

This in response to my request to return the kit to hackster.io - I have no problem logging into any nxp resource now.

"It looks like he is trying to pair multiple smartphone devices to the kit. This is not supported in the current OOB, only one smartphone can be provisioned with the UUID of the device. Regarding the account creation Idk the issue, is he experiencing issue with SSO login to rapid iot studio? He could post on NXP community if he needs helps. If he is experiencing hardware issue we should check on our log file of the part. For that we need the part number of the device. "

 

The part number is SLN-RPK-NODE  and bluetooth M 00603700000AAFEF     ID 410384939406069B

ラベル(1)
1 解決策
2,872件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

You need to upload .bin and not .atmo file

The .atmo is a file to share project to someone. The file you need to load in usb-mass-storage is the binary file generated after compile & Program Firmeware:

pastedImage_2.png

pastedImage_1.png

元の投稿で解決策を見る

5 返答(返信)
2,872件の閲覧回数
cswiger
Contributor II

Yes - have tried the reset button on the back - etc. 

If I hold SW3 while resetting we get the mass storage mode OK - oddly there is not enough room for the file:

1010739 Dec 27 08:53 Rapid IoT Kit Out Of Box Demo.atmo      < --  1MB file

Filesystem                    Size  Used Avail  Use% Mounted on

/dev/sdb                        892K 0       892K 0%     /media/chuck/RPK         < -- 900K storage 

If I try one of the smaller ones like

18238 Dec 27 08:57 Rapid IoT Blinking an LED.atmo      < -- 18K fits

and copy it on the storage it *does not* automatically reboot  as stated in the video - when manually reset it goes back to the oob demo just as before.

What is interesting is when trying to provision it the app finds the device ok, BLE blinks a few times,  IT ACTUALLY GETS THE CORRECT TIME shown on the display then RESETS, and can never attach and get data again. Like it is almost starting to work until the reset then never re-connects. 

Also, another clue, I can re-provision the same device over and over, finds it again as a new kit and adds it to the list, resets and never connects again. 

0 件の賞賛
返信
2,873件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

You need to upload .bin and not .atmo file

The .atmo is a file to share project to someone. The file you need to load in usb-mass-storage is the binary file generated after compile & Program Firmeware:

pastedImage_2.png

pastedImage_1.png

2,872件の閲覧回数
cswiger
Contributor II

Thank you sir - reflashing a new build of OOB cured the BLE connect issue - it is now getting data from the device to the phone now. 

0 件の賞賛
返信
2,872件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

As descriebed in the Quick start guide, reset procedure for rapid-iot is to push SW5 on the back of the kit with the tool included in the package.

If you mean reset default application binarys and bootloaders of the kit you can take a look at these how-to guide :

Recovering k64f &amp; kw41z applications binaries 

Recovering k64f &amp; kw41z bootloaders binaries 

You cal also try from online IDE to compile and download new binary of Out Of Box Demo and flash it to rapid-iot in usb-mass-storage mode (see this video to enter usb-mass-storage mode). This is another way to reset default OOB application.

Regards,

0 件の賞賛
返信
2,872件の閲覧回数
frakman
Contributor II

Sorry to hijack this thread and if this is an obvious question.

What is the procedure to shutdown (i.e. power off) the device? I know that you push two buttons to enter programming mode and push SW5 and reset button to reset. However, I didn't see a shutdown method mentioned anywhere. 

0 件の賞賛
返信