Cannot download RAPID-IOT-EXAMPLES.zip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot download RAPID-IOT-EXAMPLES.zip

ソリューションへジャンプ
6,224件の閲覧回数
yoursunny
Contributor III

I want to download the attachment from NXP RAPID-IOT-KIT EXAMPLES PROJECTS. However, the system says This file contains a virus or malware. The file has been deleted..

Can you upload the source code to GitHub instead? It would also be beneficial to read the code without downloading.

ラベル(1)
0 件の賞賛
返信
1 解決策
5,729件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

Upload did not work corectly, sorry for that. Please find the source code on that repo:

GitHub - theophieleroy/rapid_iot_mcuxpresso_examples 

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
5,730件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

Upload did not work corectly, sorry for that. Please find the source code on that repo:

GitHub - theophieleroy/rapid_iot_mcuxpresso_examples 

Regards,

0 件の賞賛
返信
5,729件の閲覧回数
yoursunny
Contributor III

The GitHub link works!

My experience so far (commit a1abcc96b1fca33caee172b31eb09d93e288c0bd):

SDK not found warning

When I import the project, a dialog appears:
Image 1.png

After confirming the active selection (there are no other selections), the import completes. Question: is this warning harmful?

_sdk_work wrong path

When I click Build in Quickstart Panel, the console shows this error
*** No rule to make target 'C://_sdk_work/repo-directory/iot-rpk/utilities/fsl_assert.c', needed by 'utilities/fsl_assert.o'.

I grep'ed for _sdk_work and found a reference in boards/rapidiotk64f/demo_apps/ble_sensors/.project. In this file under /projectDescription/variableList key, I changed both value to $%7BPARENT-4-PROJECT_LOC%7D, and the code compiles.

Uploading boards/rapidiotk64f/demo_apps/ble_sensors/Debug/ble_sensors.bin to the kit works.

0 件の賞賛
返信
5,729件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

Thanks for this feedback. Fix has been push to the repo.

You can ignore this warning, this is not harmfull.

Regards,

0 件の賞賛
返信
5,729件の閲覧回数
yoursunny
Contributor III

The problem is NOT SOLVED.

The downloaded ZIP file is INCOMPLETE and does not have the described examples. It contains a __All_Errors.txt file that says:

Some files weren't downloaded. The limit of file downloads has been reached. The total number of file downloads cannot be greater than 200
0 件の賞賛
返信
5,729件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

Problem solved you can now download the file on the original post.

0 件の賞賛
返信
5,729件の閲覧回数
ralphjy
Contributor II

When I download the RAPID-IOT_EXAMPLES.zip file I also get an error file that says: "Some files weren't downloaded. The limit of file downloads has been reached. The total number of file downloads cannot be greater than 200".  When I go to import the examples the instructions do not match what I see in the IDE Import Projects from File System form.  I am using IDE v10.3.0.  I also cannot see the examples that are listed in your post.

0 件の賞賛
返信
5,729件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

The issue has been raised and is being adressed as we speak by security team. We will keep you inform on the advancement. 

Theophile

0 件の賞賛
返信
5,729件の閲覧回数
yoursunny
Contributor III

In the meanwhile, can you upload the code to GitHub? It’s much easier to access because I can read code anywhere without needing a computer.

0 件の賞賛
返信