p1022 cpu up timeout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

p1022 cpu up timeout

1,468 次查看
rinkutakkar
Contributor I

We are using P1022 in our design. In one of the boards core 1 does not boot up and following print is being displayed :-

"CPU up timeout. CPU up mask is 1 should be 3".

Please guide about the possible reasons for the same.

0 项奖励
回复
3 回复数

1,378 次查看
ufedor
NXP Employee
NXP Employee

The issue corresponds to incorrect processor powering.

It is required to doublecheck the design referring the processor's Hardware Specifications and Design Checklist.

0 项奖励
回复

1,379 次查看
rinkutakkar
Contributor I

Thanks for your comments.

We have now configured this as P1013 by keeping the test_sel pin low and it is working properly.

We have checked all the power and clock rails and POR settings and they are as per processor specifications.

Kindly guide

0 项奖励
回复

1,379 次查看
ufedor
NXP Employee
NXP Employee

Please create a Technical Case - reference:

https://community.freescale.com/thread/381898 

0 项奖励
回复