effective RAM size on P2041

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

effective RAM size on P2041

2,493件の閲覧回数
emintz
Contributor I

Hi everybody,

I use P2041RDB. My RTOS kernel (loaded as elf image) occupies only 120 MB of the RAM memory. How can I configure u-boot

to initialize and use only 256MB instead of available 2GB on the board.

Thanks,

Eli

0 件の賞賛
返信
3 返答(返信)

2,342件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

It is not clear what is "effective RAM size". I think u-boot should initiate all 2GB even in case when it is possible to init only 256 MB from 2GB physically. It is not possible on the P2041RDB with single 2GB SODIMM.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,342件の閲覧回数
emintz
Contributor I

Hi Serguei,

You mean if I change RAM size in the configuration file P2041RDB.h, any changes would happen ?

Eli

0 件の賞賛
返信

2,342件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Eli Mintz,

I think you would like to change the memory mapping and the MMU setting in board\freescale\p1_p2_rdb_pc\Law.c and board\freescale\p1_p2_rdb_pc\Tlb.c.

Regards

Lunmin

0 件の賞賛
返信