Hi All,
Not getting any reply.
I am able to install sysbench package in the "fsl-full-rootfs". Following important steps i did to install the sysbech package.
1) Download sysbench package for the ppc architecture.
2) Download all dependencies of same.
3) untar ipk or rpm packages.
4) Keep in the respective folders of the file system.
It will able to run the tools.
I have tried to build the FS with open embedded yocto project provided by freescale. But sysbench bitbake not available in the repo.
I am providing this info, if any other also tried for same will help.
Thanks.