differences between Rev1 LX2160A_RDB and Rev2 LX2160A_RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

differences between Rev1 LX2160A_RDB and Rev2 LX2160A_RDB

Jump to solution
3,092 Views
jean-christoph8
Contributor I

Hello,

I try to explain why a BSP boots correctly on Rev2 LX2160A_RDB but not on a Rev1 LX2160A_RDB so I am looking for differences between those two board revisions (hardware, software, Uboot versions etc...).

Is there a way to have a list of those differences so we can try to solve this problem?

 

Many thanks in advance,

best regards

Labels (1)
0 Kudos
Reply
1 Solution
3,084 Views
ufedor
NXP Employee
NXP Employee

Rev1 LX2160A_RDB has LX2160A Rev1.0 soldered and Rev2 has LX2160A Rev2.0.

The request is not fully clear because Rev1.0 is obsolete and is not supported in two latest LSDK revisions.

View solution in original post

1 Reply
3,085 Views
ufedor
NXP Employee
NXP Employee

Rev1 LX2160A_RDB has LX2160A Rev1.0 soldered and Rev2 has LX2160A Rev2.0.

The request is not fully clear because Rev1.0 is obsolete and is not supported in two latest LSDK revisions.