differences between Rev1 LX2160A_RDB and Rev2 LX2160A_RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

differences between Rev1 LX2160A_RDB and Rev2 LX2160A_RDB

ソリューションへジャンプ
3,198件の閲覧回数
jean-christoph8
Contributor I

Hello,

I try to explain why a BSP boots correctly on Rev2 LX2160A_RDB but not on a Rev1 LX2160A_RDB so I am looking for differences between those two board revisions (hardware, software, Uboot versions etc...).

Is there a way to have a list of those differences so we can try to solve this problem?

 

Many thanks in advance,

best regards

ラベル(1)
0 件の賞賛
返信
1 解決策
3,190件の閲覧回数
ufedor
NXP Employee
NXP Employee

Rev1 LX2160A_RDB has LX2160A Rev1.0 soldered and Rev2 has LX2160A Rev2.0.

The request is not fully clear because Rev1.0 is obsolete and is not supported in two latest LSDK revisions.

元の投稿で解決策を見る

1 返信
3,190件の閲覧回数
ufedor
NXP Employee
NXP Employee

Rev1 LX2160A_RDB has LX2160A Rev1.0 soldered and Rev2 has LX2160A Rev2.0.

The request is not fully clear because Rev1.0 is obsolete and is not supported in two latest LSDK revisions.