Why LSDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why LSDK?

1,926 Views
dougbailey
Contributor III

I have software on multiple platforms that are built using Yocto.  I am looking now at the possibility of using Layerscape but noticed that it's emphasis is on using LSDK.  

Why would I use LSDK which requires me to learn yet another development environment and requires me to maintain recipes in both Yocto and LSDK? 

Regards, 

Doug Bailey 

1 Reply

1,744 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

I think it is a rhetorical question. This introduction says that LSDK meets market demand to more Linux distributions of more types, and satisfy the requirement from a wide variety of customers. It also  provides comparison between LSDK and Yocto SDK. By the way Yocto SDK also supports Layerscape QorIQ devices.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply