Why LSDK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why LSDK?

1,927件の閲覧回数
dougbailey
Contributor III

I have software on multiple platforms that are built using Yocto.  I am looking now at the possibility of using Layerscape but noticed that it's emphasis is on using LSDK.  

Why would I use LSDK which requires me to learn yet another development environment and requires me to maintain recipes in both Yocto and LSDK? 

Regards, 

Doug Bailey 

1 返信

1,745件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

I think it is a rhetorical question. This introduction says that LSDK meets market demand to more Linux distributions of more types, and satisfy the requirement from a wide variety of customers. It also  provides comparison between LSDK and Yocto SDK. By the way Yocto SDK also supports Layerscape QorIQ devices.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信