Use Secure Engine on LS1043A for Security boot and cryptography

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Use Secure Engine on LS1043A for Security boot and cryptography

1,695 次查看
Xiaomingtang
Contributor I

Hello,

I want use the secure engine hardware on LS1043A for AES and RNG. There is CAAM driver in the Linux Kernel, which provide access to the hardware via DMA. My problem is I want use it in the stand alone image, like boot loader and Uboot, which doesn't have Linux OS.  Does anyone know is there is stand alone lib code or Can I use and link Caam driver code directly with Uboot code? 

Thanks.

Xiaoming

0 项奖励
回复
2 回复数

1,689 次查看
Xiaomingtang
Contributor I

Is it possible to use Caam code with no or mini modification? Like calling the caam_jr_init() in jr.c  to init hardware.

0 项奖励
回复

1,691 次查看
ufedor
NXP Employee
NXP Employee

Currently there is no such library.

Please consider using payed NXP Professional Engineering Services:

https://contact.nxp.com/ps2019

0 项奖励
回复