Use Secure Engine on LS1043A for Security boot and cryptography

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use Secure Engine on LS1043A for Security boot and cryptography

1,670 Views
Xiaomingtang
Contributor I

Hello,

I want use the secure engine hardware on LS1043A for AES and RNG. There is CAAM driver in the Linux Kernel, which provide access to the hardware via DMA. My problem is I want use it in the stand alone image, like boot loader and Uboot, which doesn't have Linux OS.  Does anyone know is there is stand alone lib code or Can I use and link Caam driver code directly with Uboot code? 

Thanks.

Xiaoming

0 Kudos
Reply
2 Replies

1,664 Views
Xiaomingtang
Contributor I

Is it possible to use Caam code with no or mini modification? Like calling the caam_jr_init() in jr.c  to init hardware.

0 Kudos
Reply

1,666 Views
ufedor
NXP Employee
NXP Employee

Currently there is no such library.

Please consider using payed NXP Professional Engineering Services:

https://contact.nxp.com/ps2019

0 Kudos
Reply