Use Secure Engine on LS1043A for Security boot and cryptography

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use Secure Engine on LS1043A for Security boot and cryptography

1,696件の閲覧回数
Xiaomingtang
Contributor I

Hello,

I want use the secure engine hardware on LS1043A for AES and RNG. There is CAAM driver in the Linux Kernel, which provide access to the hardware via DMA. My problem is I want use it in the stand alone image, like boot loader and Uboot, which doesn't have Linux OS.  Does anyone know is there is stand alone lib code or Can I use and link Caam driver code directly with Uboot code? 

Thanks.

Xiaoming

0 件の賞賛
返信
2 返答(返信)

1,690件の閲覧回数
Xiaomingtang
Contributor I

Is it possible to use Caam code with no or mini modification? Like calling the caam_jr_init() in jr.c  to init hardware.

0 件の賞賛
返信

1,692件の閲覧回数
ufedor
NXP Employee
NXP Employee

Currently there is no such library.

Please consider using payed NXP Professional Engineering Services:

https://contact.nxp.com/ps2019

0 件の賞賛
返信