USB hotplug is not working if CONFIG_PM is enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB hotplug is not working if CONFIG_PM is enabled

1,787 Views
vm18553
Contributor II

Hello,

I'm facing an issue with USB detection when CONFIG_PM is enabled.

With CONFIG_PM=y, USB enumeration works fine if USB is connected to the device before power on, If USB is connected to the device after power on, no USB related message is seen in dmeg . 

If CONFIG_PM=n, then USB just works fine.

I'm using Freescale LS1021A, kernel - 4.14.53-rt34.

Any help is appreciated.

 

Thanks,

Vishnu

0 Kudos
Reply
1 Reply

1,775 Views
Pavel
NXP Employee
NXP Employee

This setting is enabled in NXP SDK/LSDK. See the power-management.txt in /Documentation folder.

0 Kudos
Reply