USB hotplug is not working if CONFIG_PM is enabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB hotplug is not working if CONFIG_PM is enabled

1,793件の閲覧回数
vm18553
Contributor II

Hello,

I'm facing an issue with USB detection when CONFIG_PM is enabled.

With CONFIG_PM=y, USB enumeration works fine if USB is connected to the device before power on, If USB is connected to the device after power on, no USB related message is seen in dmeg . 

If CONFIG_PM=n, then USB just works fine.

I'm using Freescale LS1021A, kernel - 4.14.53-rt34.

Any help is appreciated.

 

Thanks,

Vishnu

0 件の賞賛
返信
1 返信

1,781件の閲覧回数
Pavel
NXP Employee
NXP Employee

This setting is enabled in NXP SDK/LSDK. See the power-management.txt in /Documentation folder.

0 件の賞賛
返信