USB hotplug is not working if CONFIG_PM is enabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB hotplug is not working if CONFIG_PM is enabled

1,797 次查看
vm18553
Contributor II

Hello,

I'm facing an issue with USB detection when CONFIG_PM is enabled.

With CONFIG_PM=y, USB enumeration works fine if USB is connected to the device before power on, If USB is connected to the device after power on, no USB related message is seen in dmeg . 

If CONFIG_PM=n, then USB just works fine.

I'm using Freescale LS1021A, kernel - 4.14.53-rt34.

Any help is appreciated.

 

Thanks,

Vishnu

标记 (4)
0 项奖励
回复
1 回复

1,785 次查看
Pavel
NXP Employee
NXP Employee

This setting is enabled in NXP SDK/LSDK. See the power-management.txt in /Documentation folder.

0 项奖励
回复