UART plex!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART plex!

Jump to solution
2,934 Views
qammarabbas
Contributor IV

Hi,

T1042 processor has 2 DUART modules, and a total of 4 UARTs. Are the 4 UARTs full duplex? Or are they simplex?

Tags (1)
0 Kudos
Reply
1 Solution
1,629 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

The 4 UARTs are full duplex.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,630 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

The 4 UARTs are full duplex.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply