U-Boot compilation error - Old GCC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

U-Boot compilation error - Old GCC

4,816件の閲覧回数
shamanth_kudali
Contributor II

I am trying to build U-boot for LS1046ARDB (ls104ardb_emmc_defconfig) using the Linux SDK (2.0). 

I am getting the following error:

make
scripts/kconfig/conf --syncconfig Kconfig
CHK include/config.h
UPD include/config.h
CFG u-boot.cfg
GEN include/autoconf.mk
GEN include/autoconf.mk.dep
CFG spl/u-boot.cfg
GEN spl/include/autoconf.mk
*** Your GCC is older than 6.0 and is not supported. 

Please note:

My OS is Ubuntu 14.04 because I followed the instructions provided by NXP on this Build error SDK v1.8  to build the Linux SDK.

But this, Build U-Boot fails with "Your GCC is older than 6.0 ..." 
suggests me to use Ubuntu 18. 

How can I get the GCC update without updating my Ubuntu OS? 

Please help. 

Thanks,

Shamanth

0 件の賞賛
返信
2 返答(返信)

3,815件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Shamanth Kudaligi Pranesharao,

Please install the Cross compiler provided in SDK 2.0 on your host machine to build LS1046ARDB u-boot, it is not related with the local GCC environment on your host.

Please download Linux SDK image ISO for AARCH64 QorIQ-SDK-V2.0-AARCH64-IMAGE-20160527-yocto.iso from Linux® SDK for QorIQ® Processors | NXP.

Please run the script in folder fsl-toolchain to install Toolchain in folder /opt/fsl-qoriq/2.0/.

Build u-boot with the following commands

$ source /opt/fsl-qoriq/2.0/environment-setup-aarch64-fsl-linux

$ make CROSS_COMPILE=aarch64-fsl-linux- ls1046ardb_emmc_defconfig

$ make -j 4  CROSS_COMPILE=aarch64-fsl-linux- all


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,815件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Shamanth,

 

Today I also reproduced your problem when using SDK 2.0 Toolchain to build the latest LSDK 1812 u-boot.

The recent released u-boot requires the cross compiler GCC is upper than 6.0, I uploaded GCC compiler 8.2 installer file for ARMv8 here "https://drive.google.com/open?id=1eMNGSGJLdmqig7ILy6JVesncD_8wMpbZ", you could download and install it then build u-boot with the following commands.

$ source ~/toolchain/environment-setup-aarch64-fsl-linux

$ cd u-boot
$ make CROSS_COMPILE=aarch64-fsl-linux- ls1046ardb_emmc_defconfig
$ make -j 4  CROSS_COMPILE=aarch64-fsl-linux- all


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------