TA_PROG_SFP PIN for secure boot fuse programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TA_PROG_SFP PIN for secure boot fuse programming

ソリューションへジャンプ
2,612件の閲覧回数
mauromoioli
Contributor I

Hi all,

we are working on a new board based on LS1012A SOC that includes secure boot feature. The TA_PROG_SFP PIN that enables secure boot has to be powered with 1.8V to burn internal fuses.

According to the LS1012A DS, "For all other operating conditions, TA_PROG_SFP must be tied to GND.". This create a manufacturing issue since we need to program the board and then, rework it with a 0ohm.

Here my questions:

1. Is it acceptable to tie TA_PROG_SFP to GND by a 100ohm resistor?

2. What would be the maximum resistor value?

Thank in advance for your support.

M.

0 件の賞賛
返信
1 解決策
2,432件の閲覧回数
ufedor
NXP Employee
NXP Employee

300 Ohm resistors are used on NXP development boards.

It is recommended implementing the same way.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,433件の閲覧回数
ufedor
NXP Employee
NXP Employee

300 Ohm resistors are used on NXP development boards.

It is recommended implementing the same way.

0 件の賞賛
返信