TA_PROG_SFP PIN for secure boot fuse programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TA_PROG_SFP PIN for secure boot fuse programming

Jump to solution
2,607 Views
mauromoioli
Contributor I

Hi all,

we are working on a new board based on LS1012A SOC that includes secure boot feature. The TA_PROG_SFP PIN that enables secure boot has to be powered with 1.8V to burn internal fuses.

According to the LS1012A DS, "For all other operating conditions, TA_PROG_SFP must be tied to GND.". This create a manufacturing issue since we need to program the board and then, rework it with a 0ohm.

Here my questions:

1. Is it acceptable to tie TA_PROG_SFP to GND by a 100ohm resistor?

2. What would be the maximum resistor value?

Thank in advance for your support.

M.

0 Kudos
Reply
1 Solution
2,427 Views
ufedor
NXP Employee
NXP Employee

300 Ohm resistors are used on NXP development boards.

It is recommended implementing the same way.

View solution in original post

0 Kudos
Reply
1 Reply
2,428 Views
ufedor
NXP Employee
NXP Employee

300 Ohm resistors are used on NXP development boards.

It is recommended implementing the same way.

0 Kudos
Reply