T2081 JTAG Testing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2081 JTAG Testing

38,125 Views
hemanttiwari199
Contributor III

Dear All,

We have designed customize T2081 based SBC. Now we want to check whether the JTAG in our board is working or not using code warrior?

Can you please provide step by step guidelines or any document to check the working of our custom board JTAG using code warrior?

Regards

Hemant

 

Tags (4)
0 Kudos
Reply
22 Replies

757 Views
ufedor
NXP Employee
NXP Employee

> What is the procedure to flash internal SRAM of T2081?

There is no way to "flash" internal SRAM because it is a volatile memory.

0 Kudos
Reply

752 Views
hemanttiwari199
Contributor III

Hi,

Can we write some data into SRAM of T2081 while connecting via JTAG. FYI This is custom T2081 board which is configured to RCW setting?

Regards

0 Kudos
Reply