T2080 Sata Reference Clock Requirements

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 Sata Reference Clock Requirements

1,503 次查看
william_buder
Contributor I

Hi,

I have a question about the jitter requirements for the T2080 Sata reference clock. In table 94 or the latest data sheet a phase jitter(Peak-to-peak) of +/- 50 ps is required. Note 3. then specifies that this is only the the frequency bands of 150kHz to 15MHz at a BER of 10^-12. 

To accurately measure this would the procedure be to take the RMS jitter for that frequency range, then multiply it by a factor of 14.069 for a BER of 10^-12. In our system we are using the following clock source from IDT 9FGV0841AKILF. When measuring the RMS jitter we get 11.368ps. Converting to a Phase jitter of 159.936ps. Is this the correct method to determine whether or not that requirement is being met?

Thanks,

Will

标记 (1)
0 项奖励
回复
1 回复

1,377 次查看
r8070z
NXP Employee
NXP Employee

It is specified as +/- 50 ps, hence your RMS result should be multiplied by +/- 7 for comparing. I.e. you get ~80 ps which is greater then required.