[T1040RDB] Test reflector -> error: failed to load configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[T1040RDB] Test reflector -> error: failed to load configuration

3,411 Views
nicolaskury
Contributor II

Hi

I have a T1040RDB and I would like to try the example with reflector. I follow the documentation :

<qoriqsdk1.7_path>/sdk_documentation/4099560.html

I start the board with the default image fsl-core. The logs :

log

Net:   Initializing Fman

Fman1: Uploading microcode version 106.4.14

FSL_MDIO0:0 is connected to FM1@DTSEC1.  Reconnecting to FM1@DTSEC2

FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5

...

## Booting kernel from Legacy Image at e8020000 ...

   Image Name:   Linux-3.12.19-rt30-QorIQ-SDK-V1.

   Image Type:   PowerPC Linux Kernel Image (gzip compressed)

   Data Size:    4351614 Bytes = 4.2 MiB

...

## Loading init Ramdisk from Legacy Image at e9300000 ...

   Image Name:   fsl-image-core-t1040rdb-20141214

   Image Type:   PowerPC Linux RAMDisk Image (gzip compressed)

   Data Size:    29372982 Bytes = 28 MiB

....

No USDPAA memory, no 'usdpaa_mem' bootarg

...

dpaa_debugfs: FSL DPAA Ethernet debugfs entries ()

dpaa_generic_debugfs: FSL DPAA Ethernet debugfs entries ()

fsl_mac: fsl_mac: FSL FMan MAC API based driver ()

fsl_mac ffe4e0000.ethernet: FMan MEMAC

fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:04:9f:03:43:75

fsl_mac ffe4e2000.ethernet: FMan MEMAC

fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:04:9f:03:43:76

fsl_mac ffe4e4000.ethernet: FMan MEMAC

fsl_mac ffe4e4000.ethernet: FMan MAC address: 00:04:9f:03:43:77

fsl_mac ffe4e6000.ethernet: FMan MEMAC

fsl_mac ffe4e6000.ethernet: FMan MAC address: 00:04:9f:03:43:78

fsl_mac ffe4e8000.ethernet: FMan MEMAC

fsl_mac ffe4e8000.ethernet: FMan MAC address: 00:04:9f:03:43:79

fsl_dpa: FSL DPAA Ethernet driver ()

fsl_dpa: fsl_dpa: Probed interface eth0

fsl_dpa: fsl_dpa: Probed interface eth1

fsl_dpa: fsl_dpa: Probed interface eth2

fsl_dpa: fsl_dpa: Probed interface eth3

fsl_dpa: fsl_dpa: Probed interface eth4

...

Then:

cd /usr/etc

fmc -c usdpaa_config_t1_serdes_0x66.xml -p usdpaa_policy_hash_ipv4.xml -a

killall l2sw_bin

/etc/init.d/l2switch start

l2switch-cfg  mac add 00:11:22:33:44:01 0   #(Add mac address to FDB of port 0)

l2switch-cfg  mac add 00:11:22:33:55:01 1

l2switch-cfg  mac add 00:11:22:33:44:02 2

l2switch-cfg  mac add 00:11:22:33:55:02 3

l2switch-cfg  mac add 00:11:22:33:44:03 4

l2switch-cfg  mac add 00:11:22:33:55:03 4

l2switch-cfg  mac add 00:04:9f:03:43:75 8   # replace <...> with real MAC address

l2switch-cfg  mac add 00:04:9f:03:43:75 9   # replace <...> with real MAC address

l2switch-cfg  mac dump

mac dump
TypeVID  MAC Address    Ports

------  ---  -----------------  -----

Static  100:04:9f:03:43:75  9
Static  100:11:22:33:44:01  0
Static  100:11:22:33:44:02  2
Static  100:11:22:33:44:03  4
Static  100:11:22:33:55:01  1
Static  100:11:22:33:55:02  3
Static  100:11:22:33:55:03  4

Static  entries: 7

Dynamic entries: 0

First "problem", my entry for port 8 is missing, but anyway. Then :

reflector 3 -c usdpaa_config_t1_serdes_0x66.xml -p usdpaa_policy_hash_ipv4.xml -d 0x10000000

Found /fsl,dpaa/dpa-fman0-oh@2, Tx Channel = 80a, FMAN = 0, Port ID = 1

apps/lib/usdpaa_netcfg_layer.c:577:usdpaa_netcfg_acquire(): fmc_netcfg_get_info()

error: failed to load configuration

I don't understand what I'm doing wrong...

Thank you

0 Kudos
Reply
3 Replies

2,389 Views
nicolaskury
Contributor II

Hi

I updated Fman with fsl_fman_ucode_t1040_r1.0_107_4_2.bin and rcw with rcw_1400MHz. I

Fman1: Uploading microcode version 107.4.2

FSL_MDIO0:0 is connected to FM1@DTSEC1.  Reconnecting to FM1@DTSEC2

FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5

Hit any key to stop autoboot:  0

I reserved also some memory

nohvboot=tftp 1000000 $dir/$bootfile;tftp 2000000 $dir/$ramdiskfile;tftp c00000 $dir/$fdtfile;setenv bootargs root=/dev/ram rw console=ttyS0,115200 $othbootargs;bo;

I sill don't understand why it fails

root@t1040rdb:/usr/etc#  reflector 3 -c usdpaa_config_t1_serdes_0x66.xml -p usdpaa_policy_hash_ipv4.xml -d 0x10000000

Found /fsl,dpaa/dpa-fman0-oh@2, Tx Channel = 80a, FMAN = 0, Port ID = 1

lib/syscfg/usdpaa_netcfg_layer.c:577:usdpaa_netcfg_acquire(): fmc_netcfg_get_info()

error: failed to load configuration

Thank you

0 Kudos
Reply

2,389 Views
nicolaskury
Contributor II

Hi

Thank you for the answer. I still have error...

1) i gave some memory :

=> printenv

baudrate=115200

bdev=sda3

boot=run my_dtb my_fs my_kern my_boot

bootargs=root=/dev/ram rw console=ttyS0,115200 ramdisk_size=700000

bootcmd=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;bootm e8020000 e9300000 e8800000

bootdelay=3

bootfile=uImage

c=ffe

consoledev=ttyS0

eth1addr=00:04:9F:03:43:76

eth2addr=00:04:9F:03:43:77

eth3addr=00:04:9F:03:43:78

eth4addr=00:04:9F:03:43:79

eth5addr=00:04:9f:8e:7b:b4

ethact=FM1@DTSEC1

ethaddr=00:04:9F:03:43:75

ethprime=e1000#0

fdtaddr=c00000

fdtfile=uImage-t1040rdb.dtb

fileaddr=c00000

filesize=9a83

fman_ucode=eff00000

hvboot=setenv bootargs console=$consoledev,$baudrate config-addr=0xfe8900000;bootm 0xfe8700000 - 0xfe8800000

hwconfig=fsl_ddr:bank_intlv=cs0_cs1

ipaddr=192.168.2.105

kuryboot=tftp 0x4000000 core_edited/uRamdisk; tftp 0x1000000 core_edited/uImage--3.12-r0; tftp e8800000 core_edited/uImage--3.12-r0-t1040d4rdb.dtb; bootm 0x1000000 0x4000000 e8800000;

loadaddr=1000000

my_boot=bootm 0x1000000 0x2000000 0x0c00000

my_dtb=tftp 0x00c00000 uImage-t1040d4rdb.dtb

my_fs=tftp 0x2000000 kvm-image-extended-t1040d4rdb-64b-20151126101307.rootfs.ext4

my_kern=tftp 0x1000000 uImage_64bit.bin

netdev=eth0

nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootr

nohvboot=tftp 1000000 $dir/$bootfile;tftp 2000000 $dir/$ramdiskfile;tftp c00000 $dir/$fdtfile;setenv bootargs root=/dev/ram rw console=ttyS0,115200 $othbootargs;bootm 1000000 2000000 c00000;

othbootargs=isolcpus=1-3 usdpaa_mem=256M bportals=s0 qportals=s0 fsl_fm_max_frm=9000

ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdr

ramdiskaddr=2000000

ramdiskfile=fsl-image-flash-t1040rdb.ext2.gz.u-boot

rootpath=/opt/nfsroot

serverip=192.168.2.22

tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize && protect on $ubootaddr +$filesize && cmp.b $loadade

uboot=u-boot.bin

ubootaddr=0xeff40000

2) Yes I use the good udspaa.dtb... I took the original files provided on a usb key with the T1040.

tftp 0x4000000 sdk1.7_default/fsl-image-core-t1040rdb-64b-20141214121956.rootfs.uRamdisk

tftp 0x1000000 sdk1.7_default/uImage--3.12-r0-t1040rdb-64b-20141213100714.bin

tftp e8800000 sdk1.7_default/uImage--3.12-r0-t1040rdb-usdpaa-20141213100714.dtb

bootm 0x1000000 0x4000000 e8800000

My problem is the same as Reflector on P4080DS is not working

root@t1040rdb:/usr/etc# reflector 3 -c usdpaa_config_t1_serdes_0x66.xml -p usdpaa_policy_hash_ipv4.xml -d 0x10000000

Found /fsl,dpaa/dpa-fman0-oh@2, Tx Channel = 80a, FMAN = 0, Port ID = 1

apps/lib/usdpaa_netcfg_layer.c:577:usdpaa_netcfg_acquire(): fmc_netcfg_get_info()

error: failed to load configuration

The full log.  I should see "fsl_dpa_proxy-proxy ethernet.18: probed MAC device with MAC address: 00:e0:0c:00:27:04" but it is not the case.

=> bootm 0x1000000 0x4000000 e8800000

WARNING: adjusting available memory to 30000000

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   Linux-3.12.19-rt30-QorIQ-SDK-V1.

   Image Type:   PowerPC Linux Kernel Image (gzip compressed)

   Data Size:    5123378 Bytes = 4.9 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 04000000 ...

   Image Name:   Rootfs

   Image Type:   PowerPC Linux RAMDisk Image (gzip compressed)

   Data Size:    30738030 Bytes = 29.3 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at e8800000

   Booting using the fdt blob at 0xe8800000

   Uncompressing Kernel Image ... OK

   Loading Ramdisk to 2e2af000, end 2ffff66e ... OK

   Loading Device Tree to 03fe4000, end 03fffb65 ... OK

Warning: MAC address for l2switch not found

Using CoreNet Generic machine description

MMU: Supported page sizes

         4 KB as direct

      1024 KB as direct

      2048 KB as direct

      4096 KB as direct

     16384 KB as direct

     65536 KB as direct

    262144 KB as direct

   1048576 KB as direct

MMU: Book3E HW tablewalk not supported

Found initrd at 0xc00000002e2af000:0xc00000002ffff66e

No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using memblock_alloc(0000000000400000)

No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using memblock_alloc(0000000002000000)

Qman ver:0a01,03,01,03

No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using memblock_alloc(0000000001000000)

Bman ver:0a02,02,01

pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-pdsr', using memblock_alloc(0x0000000001000000)

pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-sre', using memblock_alloc(0x0000000000a00000)

No USDPAA memory, no 'usdpaa_mem' bootarg

bootconsole [udbg0] enabled

CPU maps initialized for 1 thread per core

Starting Linux PPC64 #1 SMP Sat Dec 13 18:31:15 HKT 2014

-----------------------------------------------------

ppc64_pft_size                = 0x0

physicalMemorySize            = 0x100000000

ppc64_caches.dcache_line_size = 0x40

ppc64_caches.icache_line_size = 0x40

-----------------------------------------------------

<- setup_system()

Linux version 3.12.19-rt30-QorIQ-SDK-V1.7+g6619b8b (jenkins@debian) (gcc version 4.8.1 (GCC) ) #1 SMP Sat Dec 13 18:31:15 HKT 2014

CF000012

Setup Arch

[boot]0012 Setup Arch

CoreNet Generic board from Freescale Semiconductor

Zone ranges:

  DMA      [mem 0x00000000-0x7fffffff]

  Normal   [mem 0x80000000-0xffffffff]

Movable zone start for each node

Early memory node ranges

  node   0: [mem 0x00000000-0xffffffff]

MMU: Allocated 2112 bytes of context maps for 255 contexts

CF000015

Setup Done

[boot]0015 Setup Done

PERCPU: Embedded 11 pages/cpu @c000000007900000 s15808 r0 d29248 u262144

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 1034240

Kernel command line: root=/dev/ram rw console=ttyS0,115200 ramdisk_size=700000

PID hash table entries: 4096 (order: 3, 32768 bytes)

Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)

Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)

Sorting __ex_table...

Memory: 3940872K/4194304K available (8020K kernel code, 1148K rwdata, 2844K rodata, 348K init, 772K bss, 253432K reserved)

Hierarchical RCU implementation.

        RCU restricting CPUs from NR_CPUS=24 to nr_cpu_ids=4.

NR_IRQS:512 nr_irqs:512 16

mpic: Setting up MPIC " OpenPIC  " version 1.2 at ffe040000, max 4 CPUs

mpic: ISU size: 512, shift: 9, mask: 1ff

mpic: Initializing for 512 sources

clocksource: timebase mult[1aaaaaab] shift[24] registered

Console: colour dummy device 80x25

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 256

mpic: requesting IPIs...

e500 family performance monitor hardware support registered

Brought up 4 CPUs

devtmpfs: initialized

xor: measuring software checksum speed

   8regs     :  3197.000 MB/sec

   8regs_prefetch:  2606.000 MB/sec

   32regs    :  3077.000 MB/sec

   32regs_prefetch:  2740.000 MB/sec

xor: using function: 8regs (3197.000 MB/sec)

NET: Registered protocol family 16

Found FSL PCI host bridge at 0x0000000ffe240000. Firmware bus number: 0->0

PCI host bridge /pcie@ffe240000  ranges:

MEM 0x0000000c00000000..0x0000000c0fffffff -> 0x00000000e0000000

  IO 0x0000000ff8000000..0x0000000ff800ffff -> 0x0000000000000000

/pcie@ffe240000: PCICSRBAR @ 0xff000000

/pcie@ffe240000: Setup 64-bit PCI DMA window

/pcie@ffe240000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.

/pcie@ffe240000: DMA window size is 0xe0000000

Found FSL PCI host bridge at 0x0000000ffe250000. Firmware bus number: 0->0

PCI host bridge /pcie@ffe250000  ranges:

MEM 0x0000000c10000000..0x0000000c1fffffff -> 0x00000000e0000000

  IO 0x0000000ff8010000..0x0000000ff801ffff -> 0x0000000000000000

/pcie@ffe250000: PCICSRBAR @ 0xff000000

/pcie@ffe250000: Setup 64-bit PCI DMA window

/pcie@ffe250000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.

/pcie@ffe250000: DMA window size is 0xe0000000

Found FSL PCI host bridge at 0x0000000ffe260000. Firmware bus number: 0->0

PCI host bridge /pcie@ffe260000  ranges:

MEM 0x0000000c20000000..0x0000000c2fffffff -> 0x00000000e0000000

  IO 0x0000000ff8020000..0x0000000ff802ffff -> 0x0000000000000000

/pcie@ffe260000: PCICSRBAR @ 0xff000000

/pcie@ffe260000: Setup 64-bit PCI DMA window

/pcie@ffe260000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.

/pcie@ffe260000: DMA window size is 0xe0000000

Found FSL PCI host bridge at 0x0000000ffe270000. Firmware bus number: 0->0

PCI host bridge /pcie@ffe270000  ranges:

MEM 0x0000000c30000000..0x0000000c3fffffff -> 0x00000000e0000000

  IO 0x0000000ff8030000..0x0000000ff803ffff -> 0x0000000000000000

/pcie@ffe270000: PCICSRBAR @ 0xff000000

/pcie@ffe270000: Setup 64-bit PCI DMA window

/pcie@ffe270000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.

/pcie@ffe270000: DMA window size is 0xe0000000

software IO TLB [mem 0x07fcb000-0x0bfcb000] (64MB) mapped at [c000000007fcb000-c00000000bfcafff]

PCI: Probing PCI hardware

fsl-pci ffe240000.pcie: PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource [io  0x10000-0x1ffff] (bus address [0x0000-0xffff])

pci_bus 0000:00: root bus resource [mem 0xc00000000-0xc0fffffff] (bus address [0xe0000000-0xefffffff])

pci_bus 0000:00: root bus resource [bus 00]

pci 0000:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)

pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring

pci 0000:00:00.0: PCI bridge to [bus 01-ff]

fsl-pci ffe250000.pcie: PCI host bridge to bus 0001:00

pci_bus 0001:00: root bus resource [io  0x21000-0x30fff] (bus address [0x0000-0xffff])

pci_bus 0001:00: root bus resource [mem 0xc10000000-0xc1fffffff] (bus address [0xe0000000-0xefffffff])

pci_bus 0001:00: root bus resource [bus 00]

pci 0001:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)

pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring

pci 0001:00:00.0: PCI bridge to [bus 01-ff]

fsl-pci ffe260000.pcie: PCI host bridge to bus 0002:00

pci_bus 0002:00: root bus resource [io  0x32000-0x41fff] (bus address [0x0000-0xffff])

pci_bus 0002:00: root bus resource [mem 0xc20000000-0xc2fffffff] (bus address [0xe0000000-0xefffffff])

pci_bus 0002:00: root bus resource [bus 00]

pci 0002:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)

pci 0002:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring

pci 0002:00:00.0: PCI bridge to [bus 01-ff]

fsl-pci ffe270000.pcie: PCI host bridge to bus 0003:00

pci_bus 0003:00: root bus resource [io  0x43000-0x52fff] (bus address [0x0000-0xffff])

pci_bus 0003:00: root bus resource [mem 0xc30000000-0xc3fffffff] (bus address [0xe0000000-0xefffffff])

pci_bus 0003:00: root bus resource [bus 00]

pci 0003:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)

pci 0003:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring

pci 0003:00:00.0: PCI bridge to [bus 01-ff]

pci 0000:00:00.0: PCI bridge to [bus 01]

pci 0000:00:00.0:   bridge window [io  0x10000-0x1ffff]

pci 0000:00:00.0:   bridge window [mem 0xc00000000-0xc0fffffff]

pci 0001:00:00.0: PCI bridge to [bus 01]

pci 0001:00:00.0:   bridge window [io  0x21000-0x30fff]

pci 0001:00:00.0:   bridge window [mem 0xc10000000-0xc1fffffff]

pci 0002:00:00.0: PCI bridge to [bus 01]

pci 0002:00:00.0:   bridge window [io  0x32000-0x41fff]

pci 0002:00:00.0:   bridge window [mem 0xc20000000-0xc2fffffff]

pci 0003:00:00.0: PCI bridge to [bus 01]

pci 0003:00:00.0:   bridge window [io  0x43000-0x52fff]

pci 0003:00:00.0:   bridge window [mem 0xc30000000-0xc3fffffff]

bio: create slab <bio-0> at 0

raid6: int64x1    526 MB/s

raid6: int64x2    858 MB/s

raid6: int64x4   1177 MB/s

raid6: int64x8    975 MB/s

raid6: using algorithm int64x4 (1177 MB/s)

raid6: using intx1 recovery algorithm

vgaarb: loaded

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

EDAC MC: Ver: 3.0.0

Bman err interrupt handler present

Bman portal initialised, cpu 0

Bman portal initialised, cpu 1

Bman portal initialised, cpu 2

Bman portal initialised, cpu 3

Bman portals initialised

Qman err interrupt handler present

QMan: Allocated lookup table at 8000000000000000, entry count 65537

Qman portal initialised, cpu 0

Qman portal initialised, cpu 1

Qman portal initialised, cpu 2

Qman portal initialised, cpu 3

Qman portals initialised

Bman: BPID allocator includes range 32:32

Qman: FQID allocator includes range 256:512

Qman: FQID allocator includes range 32768:32768

Qman: CGRID allocator includes range 0:256

Qman: pool channel allocator includes range 1025:15

fsl-ifc ffe124000.localbus: Freescale Integrated Flash Controller

Switched to clocksource timebase

NET: Registered protocol family 2

TCP established hash table entries: 32768 (order: 7, 524288 bytes)

TCP bind hash table entries: 32768 (order: 7, 524288 bytes)

TCP: Hash tables configured (established 32768 bind 32768)

TCP: reno registered

UDP hash table entries: 2048 (order: 4, 65536 bytes)

UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

rootfs image is not initramfs (no cpio magic); looks like an initrd

Freeing initrd memory: 30016K (c00000002e2af000 - c00000002ffff000)

HugeTLB registered 1 MB page size, pre-allocated 0 pages

HugeTLB registered 4 MB page size, pre-allocated 0 pages

HugeTLB registered 16 MB page size, pre-allocated 0 pages

HugeTLB registered 64 MB page size, pre-allocated 0 pages

HugeTLB registered 256 MB page size, pre-allocated 0 pages

HugeTLB registered 1 GB page size, pre-allocated 0 pages

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

NTFS driver 2.1.30 [Flags: R/O].

jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.

msgmni has been set to 7755

async_tx: api initialized (async)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

Freescale Display Interface Unit (DIU) framebuffer driver

fsl_diu_perpare: Borad not support DIU. Can't dispaly video.

Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36, base_baud = 18750000) is a 16550A_FSL64

console [ttyS0] enabled, bootconsole disabled

console [ttyS0] enabled, bootconsole disabled

serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36, base_baud = 18750000) is a 16550A_FSL64

serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37, base_baud = 18750000) is a 16550A_FSL64

serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37, base_baud = 18750000) is a 16550A_FSL64

ePAPR hypervisor byte channel driver

brd: module loaded

loop: module loaded

st: Version 20101219, fixed bufsize 32768, s/g segs 256

fsl-sata ffe220000.sata: Sata FSL Platform/CSB Driver init

scsi0 : sata_fsl

ata1: SATA max UDMA/133 irq 68

fsl-sata ffe221000.sata: Sata FSL Platform/CSB Driver init

scsi1 : sata_fsl

ata2: SATA max UDMA/133 irq 69

fe8000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00227e

Amd/Fujitsu Extended Query Table at 0x0040

  Amd/Fujitsu Extended Query version 1.3.

number of CFI chips: 1

ftl_cs: FTL header not found.

ONFI param page 0 valid

ONFI flash detected

NAND device: Manufacturer ID: 0x2c, Chip ID: 0x38 (Micron MT29F8G08ABABAWP), 1024MiB, page size: 4096, OOB size: 224

Bad block table found at page 262016, version 0x01

Bad block table found at page 261888, version 0x01

nand_read_bbt: bad block at 0x000009600000

nand_read_bbt: bad block at 0x00000c800000

4 ofpart partitions found on MTD device fff800000.flash

Creating 4 MTD partitions on "fff800000.flash":

0x000000000000-0x000000100000 : "NAND U-Boot Image"

ftl_cs: FTL header not found.

0x000000100000-0x000000200000 : "NAND DTB Image"

ftl_cs: FTL header not found.

0x000000200000-0x000000c00000 : "NAND Linux Kernel Image"

ftl_cs: FTL header not found.

0x000000c00000-0x000020000000 : "NAND RFS Image"

ftl_cs: FTL header not found.

fsl,ifc-nand fff800000.nand: IFC NAND device at 0xfff800000, bank 1

fsl_espi ffe110000.spi: master is unqueued, this is deprecated

m25p80 spi32766.0: n25q512ax3 (65536 Kbytes)

ftl_cs: FTL header not found.

fsl_espi ffe110000.spi: at 0x800008008012e000 (irq = 53)

libphy: Fixed MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

Freescale FM module (Dec 13 2014:18:27:16), FMD API version 21.1.0

Freescale FM Ports module (Dec 13 2014:18:27:21)

dpaa_debugfs: FSL DPAA Ethernet debugfs entries ()

dpaa_generic_debugfs: FSL DPAA Ethernet debugfs entries ()

fsl_mac: fsl_mac: FSL FMan MAC API based driver ()

fsl_mac ffe4e0000.ethernet: FMan MEMAC

fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:04:9f:03:43:75

fsl_mac ffe4e2000.ethernet: FMan MEMAC

fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:04:9f:03:43:76

fsl_mac ffe4e4000.ethernet: FMan MEMAC

fsl_mac ffe4e4000.ethernet: FMan MAC address: 00:04:9f:03:43:77

fsl_mac ffe4e6000.ethernet: FMan MEMAC

fsl_mac ffe4e6000.ethernet: FMan MAC address: 00:04:9f:03:43:78

fsl_mac ffe4e8000.ethernet: FMan MEMAC

fsl_mac ffe4e8000.ethernet: FMan MAC address: 00:04:9f:03:43:79

fsl_dpa: FSL DPAA Ethernet driver ()

fsl_dpa: fsl_dpa: Probed interface eth0

fsl_dpa: fsl_dpa: Probed interface eth1

fsl_dpa: fsl_dpa: Probed interface eth2

fsl_dpa: fsl_dpa: Probed interface eth3

fsl_dpa: fsl_dpa: Probed interface eth4

fsl_dpa_shared: FSL DPAA Shared Ethernet driver ()

fsl_dpa_proxy: FSL DPAA Proxy initialization driver ()

fsl_oh: FSL FMan Offline Parsing port driver ()

fsl_oh dpa-fman0-oh.24: Found OH node handle compatible with fsl,dpa-oh.

fsl_oh dpa-fman0-oh.24: Allocating 0 ingress frame queues duples

fsl_oh dpa-fman0-oh.24: OH port /soc@ffe000000/fman@400000/port@83000 enabled.

fsl_oh dpa-fman0-oh.24: Default egress frame queue: 105

fsl_oh dpa-fman0-oh.24: Default error frame queue: 104

fsl_oh dpa-fman0-oh.24: Initialized queues:

e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k

e1000e: Copyright(c) 1999 - 2013 Intel Corporation.

fsl-of-dma ffe100300.dma: dma channel dma-uio0-0 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-1 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-2 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-3 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-4 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-5 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-6 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-7 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-0 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-1 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-2 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-3 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-4 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-5 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-6 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-7 initialized

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-pci: EHCI PCI platform driver

/soc@ffe000000/usb@210000: Invalid 'dr_mode' property, fallback to host mode

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 44, io mem 0xffe210000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

ata1: No Device OR PHYRDY change,Hstatus = 0xa0000000

ata1: SATA link down (SStatus 10 SControl 300)

ata2: No Device OR PHYRDY change,Hstatus = 0x80000000

ata2: SATA link down (SStatus 10 SControl 300)

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 45, io mem 0xffe211000

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

usbcore: registered new interface driver usb-storage

i2c /dev entries driver

mpc-i2c ffe118000.i2c: timeout 1000000 us

mpc-i2c ffe118100.i2c: timeout 1000000 us

mpc-i2c ffe119000.i2c: timeout 1000000 us

mpc-i2c ffe119100.i2c: timeout 1000000 us

i2c i2c-1: Added multiplexed i2c bus 4

i2c i2c-1: Added multiplexed i2c bus 5

i2c i2c-1: Added multiplexed i2c bus 6

i2c i2c-1: Added multiplexed i2c bus 7

pca954x 1-0077: registered 4 multiplexed busses for I2C switch pca9546

md: raid6 personality registered for level 6

md: raid5 personality registered for level 5

md: raid4 personality registered for level 4

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

/soc@ffe000000/sdhc@114000: voltage-ranges unspecified

mmc0: SDHCI controller on ffe114000.sdhc [ffe114000.sdhc] using ADMA

platform caam_qi.0: Linux CAAM Queue I/F driver initialised

caam ffe300000.crypto: Entropy delay = 3200

caam ffe300000.crypto: Instantiated RNG4 SH0

caam ffe300000.crypto: Instantiated RNG4 SH1

caam ffe300000.crypto: device ID = 0x0a12040000000000 (Era 6)

caam ffe300000.crypto: job rings = 4, qi = 1

caam algorithms registered in /proc/crypto

caam_jr ffe301000.jr: registering rng-caam

caam ffe300000.crypto: fsl,sec-v5.0 algorithms registered in /proc/crypto

platform caam_qi.0: fsl,sec-v5.0 algorithms registered in /proc/crypto

Freescale USDPAA process driver

fsl-usdpaa: no region found

Freescale USDPAA process IRQ driver

fsl-pme ffe316000.pme: ver: 0x00100202

Freescale pme2 db driver

Freescale pme2 scan driver

fsl-pme2-scan: device pme_scan registered

Freescale hypervisor management driver

fsl-hv: no hypervisor found

ipip: IPv4 over IPv4 tunneling driver

TCP: cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

NET: Registered protocol family 15

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

fsl_dpa_macless: FSL DPAA MACless Ethernet driver ()

fsl_dpa_generic: FSL DPAA Generic Ethernet driver ()

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

md: Waiting for all devices to be available before autodetect

md: If you don't use raid, use raid=noautodetect

md: Autodetecting RAID arrays.

md: Scanned 0 and added 0 devices.

md: autorun ...

md: ... autorun DONE.

RAMDISK: gzip image found at block 0

usb 1-1: new high-speed USB device number 2 using fsl-ehci

usb-storage 1-1:1.0: USB Mass Storage device detected

scsi2 : usb-storage 1-1:1.0

scsi 2:0:0:0: Direct-Access     Kingston DT Ultimate G3   PMAP PQ: 0 ANSI: 6

sd 2:0:0:0: Attached scsi generic sg0 type 0

sd 2:0:0:0: [sda] 61472768 512-byte logical blocks: (31.4 GB/29.3 GiB)

sd 2:0:0:0: [sda] Write Protect is off

sd 2:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA

sda: sda1

sd 2:0:0:0: [sda] Attached SCSI removable disk

VFS: Mounted root (ext2 filesystem) on device 1:0.

devtmpfs: mounted

Freeing unused kernel memory: 348K (c000000000aa3000 - c000000000afa000)

INIT: version 2.88 booting

Starting udev

udevd[1775]: starting version 182

seville ffe800000.l2switch: Found Seville Switch, UIO device - IRQ 26, id 0x099530e9.

seville MAC address not found

Starting Bootlog daemon: bootlogd.

Populating dev cache

net.ipv4.conf.default.rp_filter = 0

net.ipv4.conf.all.rp_filter = 0

hwclock: can't open '/dev/misc/rtc': No such file or directory

Sun Dec 14 13:03:00 UTC 2014

hwclock: can't open '/dev/misc/rtc': No such file or directory

Running postinst /etc/rpm-postinsts/100-inetutils-inetd...

Running postinst /etc/rpm-postinsts/101-sysvinit-inittab...

Running postinst /etc/rpm-postinsts/102-util-linux-readprofile...

Running postinst /etc/rpm-postinsts/103-debianutils...

Running postinst /etc/rpm-postinsts/104-inetutils-tftpd...

Running postinst /etc/rpm-postinsts/105-inetutils-ftpd...

Running postinst /etc/rpm-postinsts/106-inetutils-telnetd...

update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing)

INIT: Entering runlevel: 5up links for run-postin

Configuring network interfaces... done.

Starting system message bus: dbus.

Starting Dropbear SSH server: Generating key, this may take a while...

Public key portion is:

ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQDN8wSDXMiXBaQLXs1hnEfbxk6A/LD54h4DYirPD0xY6pnCLr8GOK0rVDWUUzQJRuIu3wQ82tXnpXVyt7AcNUiz7nCGF4ERUuc06y6iV4d2RC5Nkpih05JM9pDcZ4NbQP2rhKFgd1BlffHDWuImnNpi8/HGaAKb

Fingerprint: md5 00:54:12:49:b1:5c:9e:53:f3:56:65:01:28:e2:6f:42

dropbear.

Created /var/log/l2switch

l2switch: Started L2 Switch demo app version 0.4.0

Build Date: Dec 14 2014 20:48:42

GIT Version: fsl-sdk-v1.7-rc2-dirty

hwclock: can't open '/dev/misc/rtc': No such file or directory

Starting network benchmark server: netserver.

Starting system log daemon...0

Starting kernel log daemon...0

Starting internet superserver: xinetd.

Stopping Bootlog daemon: bootlogd.

Poky (Yocto Project Reference Distro) 1.6.1 t1040rdb /dev/ttyS0

Thank you

0 Kudos
Reply

2,389 Views
bpe
NXP Employee
NXP Employee

Suggestions:

1. Give USDPAA driver some memory, 256M recommended, by specifying usdpaa_mem=256M on the kernel parameter string. See the URL below:

   https://freescale.sdlproducts.com/LiveContent/web/pub.xql?c=t&action=home&pub=QorIQ_SDK_1.9&lang=en-...

2. Make sure USDPAA was assigned some ethernet interfaces in your Device Tree. The SDK has pre-configured examples. Should be

   <your_board>-usdpaa.dtb. More details can be found here:

 

   https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-FA9433C9-E581-440F-9D...

3. For the switch port problem, the missing one seems to be the second internal connection  to FMAN, which is not enabled by default.

   Attempt to enable by hand or move to the most recent SDK.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply