T1024 Data Path Acceleration Architecture (DPAA)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 Data Path Acceleration Architecture (DPAA)

1,459 Views
kishorebolisett
Contributor I

Hi, I work for Honeywell. We are using T1024 processor in one of our program. We are having hard time understanding 'Data Path Acceleration Architecture (DPAA)' interface on this processor. I see only linux examples only, but we are looking for some example use cases (application notes) which can run on non-linux based systems. Please guide and Help.

0 Kudos
Reply
1 Reply

1,331 Views
alexander_yakov
NXP Employee
NXP Employee

For other our processors with DPAA support we offer a package of standalone software examples named "Netcomm Software", but this software does not support DPAA. However, you can look and use as reference:

NetComm Software Resources|NXP 

Hope this will be helpful.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply