Significance of FMAN micro code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Significance of FMAN micro code

3,277 次查看
veerendranathj
Contributor III

Is it necessary to use FMAN micro code to enable Ethernet interfaces in my own standalone binary/bootloader for P2041RDB..?

If yes.. how can I integrate it?

标记 (4)
0 项奖励
回复
1 回复

1,865 次查看
bpe
NXP Employee
NXP Employee

Loading microcode is essential because it controls FMAN internal RISCs. No correct operation at all is possible

if the microcode is not loaded. Microcodes are provided as binaries, they are part of QorIQ SDK. Unpack

the package named 'fm-ucode' to get the binaries. Refer to u-boot source code, file drivers/net/fm/fm.c, function

fman_upload_firmware() on how to upload the microcode.

0 项奖励
回复