t4240 tftp serverip

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

t4240 tftp serverip

1,523 次查看
varunkjayan
Contributor II

hi

i have setup the tftp server in my host system and also i have assigned ipaddr in uboot for t4240rdb and

also for my host system but

when i try for a tftp transfer it is showing serverip not set

how to set serverip for tftp can it be given random or is there a particular ip

0 项奖励
回复
1 回复

1,353 次查看
Pavel
NXP Employee
NXP Employee

Set the board's network configuration using values appropriate for your installation and then save the configuration.

For example, host IP of my PC is 192.168.2.109 and IP of our gateway is 192.168.2.64. We use the following command sequence:

=> setenv ethaddr 00:1e:59:2f:03:35

=> setenv serverip 192.168.2.109

=> setenv ipaddr 192.168.2.104

=> setenv netmask 255.255.255.0

=> setenv gatewayip 192.168.2.64

=> saveenv

=> reset

Test your connection after reset using similar command:

=> ping 192.168.2.64

=> ping 192.168.2.109


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复