Hi,
I am interfacing 8 DDR3L devices with T1042. The external pin description of T1042 DDR Controller mentions 2 clocks MCK0 and MCK1. Why is there a second clock? Can't i drive all 8 SDRAM devices with a single clock only?
Solved! Go to Solution.
> Can't i drive all 8 SDRAM devices with a single clock only?
Driving all SDRAM devices connected to the same chip-select with a single/same MCKn is a must.
Please refer to the AN3940 - Hardware and Layout Design Considerations for DDR3 SDRAM, Table 1. DDR3 designer checklist:
"46. Ensure one clock pair is used for each chip-select. The clock pair should follow the address/command/control signal groups in fly-by topology."
> Can't i drive all 8 SDRAM devices with a single clock only?
Driving all SDRAM devices connected to the same chip-select with a single/same MCKn is a must.
Please refer to the AN3940 - Hardware and Layout Design Considerations for DDR3 SDRAM, Table 1. DDR3 designer checklist:
"46. Ensure one clock pair is used for each chip-select. The clock pair should follow the address/command/control signal groups in fly-by topology."